Skip to main content
arnold_w
Senior II
March 11, 2019
Question

On what address do the Option Bytes on STM32F446 reside on?

  • March 11, 2019
  • 19 replies
  • 3775 views

I want to read the Option Bytes values from my STM32F446 in order to debug strange behavior. On what addresses do they reside? According to the Reference Manual they reside on addresses 0x1FFFC000 and 0x1FFFC008, but when I look at the implementation of HAL_FLASHEx_OBGetConfig it is reading from addresses OPTCR_BYTE0_ADDRESS, OPTCR_BYTE1_ADDRESS, OPTCR_BYTE2_ADDRESS, and OPTCR_BYTE3_ADDRESS (0x40023C14 - 0x40023C17). Can someone please clarify?

This topic has been closed for replies.

19 replies

waclawek.jan
Super User
March 11, 2019

The option register which governs the behaviour is at 0x40023C14. The option bits are loaded with values from Flash memory (i.e. from the 0x1FFFC00x adresses) at reset release. See Flash option control register (FLASH_OPTCR) in RM0390.

JW

arnold_w
arnold_wAuthor
Senior II
November 14, 2019

But what do you mean by 0x1FFFC00x addresses in flash? If I convert 0x1FFFC000 from hex to dec then I get 536854528 = 511 Mega. The flash in the STM32F446 is only 512 kBytes, not 512 MByte. How is it then possible to store something at address 0x1FFFC000 in the flash?

arnold_w
arnold_wAuthor
Senior II
March 12, 2019

Thank you.

waclawek.jan
Super User
November 15, 2019

The FLASH is not a single piece, and it is not mapped from 0x0000'0000.

FLASH in STM32 comes in several pieces, and these pieces are mapped at different addresses within the 4GB address space of STM32.

Maybe it's confusing to say that the option bytes are loaded from FLASH, and ST avoids to say this. Nevertheless, the physical implementation is FLASH (electrically erasable, electrically programmable memory), although it's not part of the 512kBy *user* FLASH array.

Similarly, what ST calls ROM (System memory), or OTP, are physically FLASH, except the former is programmed in factory and then locked, and the latter does not have the erasing circuitry connected. Again, these portions are mapped at different addresses, non-continuously.

The user FLASH is basically mapped from 0x0800'0000 upwards. If booted into this FLASH, it is mirrored at the 0x0000'0000 space (but that space can mirror also the System memory described above, or SRAM, or FMC banks, depending on SYSCFG_MEMRMP.MEM_MODE.

JW

arnold_w
arnold_wAuthor
Senior II
November 15, 2019

So, the microcontroller looks at addresses 0x40023C14 - 0x40023C17 to decide what to do. The addresses 0x40023C14 - 0x40023C17 are initialized with values from addresses 0x1FFFC000 and  0x1FFFC008 after reset. But how do I update the values at addresses 0x1FFFC000 and  0x1FFFC008? When I look inside the function HAL_FLASHEx_OBProgram all I see is writes to addresses 0x40023C14 - 0x40023C17, not 0x1FFFC000 and  0x1FFFC008. Is there another function for writing to addresses 0x1FFFC000 and  0x1FFFC008?

My end-goal is to be able to embed all my option bytes into the hex-file (so that I know with 100% certainty what option bytes a particular firmware version is running on) using a home-made function called updateOptionBytesIfNecessary(), but my first attempts at this resulted in very strange behavior (such as automatic enabling of the read protect if I connect twice in a row with ST Link Utility).

waclawek.jan
Super User
November 15, 2019

That might be right. Programming option bytes is described in Programming user option bytes subchapter of FLASH chapter (ch.3) of RM0390; the FLASH controller takes care to program the values to proper address.

Typically, option bytes are programmed together with the program, using whichever programming tool you use, e.g. STLink Utility, or CubeProgrammer. Whether the given programming tool supports having the option bytes as part of the .hex, is dependent on that particular tool, I don't believe there is a common standard obeyed by all tools out there.

JW

arnold_w
arnold_wAuthor
Senior II
November 15, 2019

Yes, there is a section detailing how to program the user option bytes. However, user option bytes only include 3 parameters: nRST_STDBY, rRST_STOP and WDG_SW. There is no section describing how to change SPRMOD, Read Protection (RDP) and nWRPi. I could look at what the HAL-functions are doing, but it's exactly those that give me the weird behavior with read protection being enabled all of a sudden...

waclawek.jan
Super User
November 15, 2019

Aren't SPRMOD, RDP and nWRPi all contained in FLASH_OPTCR, as described in chapter 3.8.6 Flash option control register (FLASH_OPTCR) of RM0390 rev.4? So I would expect they can be changed in the same way as other items in FLASH_OPTCR, i.e. nRST_STDBY, rRST_STOP and WDG_SW.

JW

arnold_w
arnold_wAuthor
Senior II
November 25, 2019

The terminology is confusing, in Table 9 "Description of the option bytes", the following text can be found:

"USER: User option byte

This byte is used to configure the following features:

Select the watchdog event: Hardware or software

Reset event when entering the

Stop mode Reset event when entering the Standby mode"

Then in section 3.6.2 "Programming user option bytes" it says:

"To run any operation on this sector..."

So does "sector" refer to the option bytes at addresses 0x1FFFC000 and 0x1FFFC008 or just the USER bits (nRST_STDBY, rRST_STOP and WDG_SW)?

waclawek.jan
Super User
November 25, 2019

IMO all bits described in Table 9 - which are also "mirrored" in FLASH_OPTCR - are subject to programming according to section 3.6.2. In other words, you program then all at once.

Terminology is always confusing - this is a live topic, with a huge amount of concepts and details, which are sometimes hard to describe precisely without resorting to excessive explanation; and with many changes as the chips are evolving and are updated and their features expanded. Users are often expected to have prior knowledge to fill out the gaps. This is not to say documentation can't or shouldn't be improved; it's just that it's a hard task. Maybe you might want to suggest particular improvements yourself.

You may not be aware of the fact that this is a primarily user driven forum, with casual ST presence. I am not ST. If you want to pick up the issue of imprecise terminology used in the manuals, maybe you want to contact ST directly, through the web support form, or through your FAE.

JW

@Imen DAHMEN​ , could perhaps 3.6.2 in RM0390 - and all other analogous chapters in other STM32 RMs - be made less ambiguous by omitting the "user" from "user option bytes", as 3.6.2. appears to refer to programming of all option bytes, whereas "user option bytes" appear to designate only a portion of the overall option bytes?

arnold_w
arnold_wAuthor
Senior II
November 25, 2019

I'm on vacation right now, but when I get back I will try to change all bits and see if I can successfully update them using the instructions in 3.6.2 (and hence, not use the HAL-functions). Thank you for your help.

waclawek.jan
Super User
November 25, 2019

@Vincent Onde​  ,

Can't this issue be clarified within an AN, together with an overview of the various features which can be enabled/disabled using the Option bits/bytes accross all the STM32 families?

JW

arnold_w
arnold_wAuthor
Senior II
December 2, 2019

Accidental double-post.