Skip to main content
MissionYE
Associate II
September 30, 2021
Question

On-Board Communication via CAN without transceiver

  • September 30, 2021
  • 7 replies
  • 6412 views

Two CANs on the same board. Can I connect CAN1TX to CAN2RX and CAN1RX to CAN2TX?

This topic has been closed for replies.

7 replies

Javier1
Principal
September 30, 2021

Never tried it myself but why not, try with some diodes and a pullup resistor.

The canbus line needs to be pulledup high when idle(pullup resistor, if your chips logic is 3v3, use 3v3 for the pullup)

The Rx and TX need to be conneted together, so we need a diode to avoid Tx lines to spill their voltage and mess with the bus.

0693W00000FB00OQAT.pnghttps://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/605836/tms320f28035-can-bus-without-transceivers-using-ecan

hit me up in https://www.linkedin.com/in/javiermuñoz/
Tesla DeLorean
Guru
September 30, 2021

Keil​ has white papers on this and on STM3

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MissionYE
MissionYEAuthor
Associate II
September 30, 2021

Thanks

Didier_G
ST Employee
May 12, 2022

The approach looks valid for low bitrates only.

Tesla DeLorean
Guru
May 12, 2022

Bob suggests it's certainly viable to 500 Kbps on small boards

https://www.keil.com/appnotes/files/apnt_236.pdf

Similar mechanics could be applied to UART single wire bus.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Didier_G
ST Employee
May 13, 2022

This speed is far from being confirmed and this trick is probably not viable in production (automotive grade, noise immunity, etc ...).

Schottky diodes with fast transient response are required. The pull-up value has probably to be decreased if the number of controllers increases, for smart edges.