Skip to main content
Hicss.2033
Associate III
December 5, 2019
Question

On a stm32f429I discovery board, which are the voltage of the SDA and SCL pin in I2C communication? May I connect it to a I2C device with 3.3 V. Thanks.

  • December 5, 2019
  • 2 replies
  • 493 views

..

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
December 5, 2019

Voltage likely closer to 3V, buys should work on 3.3V I2C device.

You could probably measure the voltage on pins also.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Hicss.2033
Associate III
December 5, 2019

Thanks for the fast answer,. I don't understant the meaning of "buys". Can you explain better?

Besides, I need of external pull-up resistors (I'm new of the matter)?