Old DMA2 bug found in new MPU STM32F427 ?
Hello,
We use
STM32Fxx MPU
in many projects
. During the development
of new equipment with STM32F427
, wehave run into this
problem:
We use
SPI
4, whichis controlled by the
DMA
. Streamer DMA2_Stream1 is used for sending, DMA2_Stream0 for reading. DMA2_Stream0 generates an interrupt, whichprocesses the
data
and restarts
transmission
(for manyreasons it is not
possible to use
cyclic DMA)
.Interrupt handler looks like this
(actually the last
version
, programhas been
completely
rewritten
,unfortunately
behavior is the same
:(void DMA2_Stream0_Irq (
)
{
...
SPI_Cmd(SPI4, DISABLE);
SPI_DMACmd(SPI4, SPI_DMAReq_Rx | SPI_DMAReq_Tx, DISABLE);
DMA_Cmd(DMA2_Stream0, DISABLE);
DMA_Cmd(DMA2_Stream1, DISABLE);
while (DMA_GetCmdStatus(DMA2_Stream0)!=DISABLE) {};
while (DMA_GetCmdStatus(DMA2_Stream1)!=DISABLE) {};
DMA_SetCurrDataCounter(DMA2_Stream0, 14);
DMA_SetCurrDataCounter(DMA2_Stream1, 14);
DMA_MemoryTargetConfig(DMA2_Stream0, MemRx, DMA_Memory_0);
DMA_MemoryTargetConfig(DMA2_Stream1, MemTx, DMA_Memory_0);
DMA_Cmd(DMA2_Stream0, ENABLE);
DMA_Cmd(DMA2_Stream1, ENABLE);
SPI_DMACmd(SPI4, SPI_DMAReq_Rx | SPI_DMAReq_Tx, ENABLE);
SPI_Cmd(SPI4, ENABLE);
}
Up to this point
everything is
ok
.
The transmission
works perfectly,
a
ll tests
of reliability and
performance
went well.
Then we
implemented a
simple
DMA
transfer
memory2memory (for the purposes of
TCP
stack). We used
DMA2_Stream7.
Separately,
both
communication works
perfectly
. If, however, are
used simultaneously
,errors occur
.DMA2_Stream0 interrupt is not called
.
It looks as
if the
SPI4
readby one character
less
than
sent
.After error, DMA2_Stream0 is enabled (and
waits
indefinitely
), hasNDTR=1 and
TCIF
=0
.
DMA2_Stream1 is stopped, has
NDTR=0 and
TCIF=1.
From these data
it is evident
why
SPI
stops working
.I remembered
that a similar
errata was
in the chip
STM32F407. And indeed,
error
occurs
only
if
source addr is FMC!!!Shortly
, if dma memory2memory is:
SRAM-
>
SRAM ... everything is
ok
SRAM-
>FMC
... everything is
ok
FMC
-
>FMC
... error
FMC
-
>
SRAM ... error
Oddly enough
, this error
is not described in
the
errata documentation.
It is
this error
and is there a
workaround
?Or am I doing
something
wrong
?