Skip to main content
Chan.Calvin
Associate III
October 14, 2024
Solved

Odd observation on STM32G071 device

Hi all

STM32CubeIDE v1.16.1

firmware package: cube FW_C0 V1.2.0

I use the IDE to start a new project with STM32G071 on its discovery board.

Just simply configure PD0, 1, 2, and 3 as inputs with pull-ups.  All other aspects are using IDE defaults.

code generated either using HAL or LL, and in the main while (1) loop just put a couple of __NOP() ; calls.

Nothing are connected externally.

Set breakpoint in mainloop __NOP() call, I am expecting PD_IDR should have pin 0 - 3 all at 1  (value 0xF), but funny enough, PD_IDR has value 0x0a.

In fact, this is observed after MX_GPIO_Init is called.

void MX_GPIO_Init(void)

{

 

GPIO_InitTypeDef GPIO_InitStruct = {0};

 

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOD_CLK_ENABLE();

 

/*Configure GPIO pins : PD0 PD1 PD2 PD3 */

GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;

GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

GPIO_InitStruct.Pull = GPIO_PULLUP;

HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 

}

Also with LL code generation, single step tracing gives

initialization of PD0 gives correct observation

then initialization of PD1 put PD0 to 0, while PD1 to 1

then initialization of PD2 gives correct observation

then initialization of PD3 put PD2 to 0, while PD3 to 1

thus the outcome of PD_IDR valued as (0xA).

void MX_GPIO_Init(void)

{

 

LL_GPIO_InitTypeDef GPIO_InitStruct = {0};

 

/* GPIO Ports Clock Enable */

LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOD);

 

/**/

GPIO_InitStruct.Pin = LL_GPIO_PIN_0;

GPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;

GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;

LL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 

/**/

GPIO_InitStruct.Pin = LL_GPIO_PIN_1;

GPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;

GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;

LL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 

/**/

GPIO_InitStruct.Pin = LL_GPIO_PIN_2;

GPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;

GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;

LL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 

/**/

GPIO_InitStruct.Pin = LL_GPIO_PIN_3;

GPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;

GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;

LL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 

}

 

I also tried on STM32C031 discovery, and it has identical observation.

Is there any area I missed out in the setup to cause this issue.

Anyone comes across this?

 

Rgd

 

Calvin

 

 

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
October 14, 2024

This is consequence of USB-C PD dead-battery support.

JW

7 replies

waclawek.jan
waclawek.janBest answer
Super User
October 14, 2024

This is consequence of USB-C PD dead-battery support.

JW

Chan.Calvin
Associate III
October 14, 2024

@JW_it 

Thank you for your pointer.  Then it is funny enough that I tried on C031C6 and get identical observation?

 

Rgds

Calvin

waclawek.jan
Super User
October 14, 2024

Well, that's weird, as the 'C0 is not supposed to have the USB-C PD support.

What hardware is this? Can you post a foto of the chip?

The 5k1 resistor can be measured between PD0-GND and PD2-GND when the chip is powered down (provided there is a logic 1 at PD1/PD3 - with some multimeters, it's enough to short PD0+PD1 with the meter's positive terminal, others don't supply enough voltage). Can you try on both chips?

JW

Chan.Calvin
Associate III
October 14, 2024

@JW_it

By the way, I am using nucleo board. nucleo-c031c6. 

As a matter of fact, I am using nucleo all the way, and not discovery as mentioned before.

 

The C031 may be carrying the gotcha from G0.

 

Rgds

 

Calvin

Karl Yamashita
Principal
October 14, 2024

@Chan.Calvin wrote:

@JW_it

By the way, I am using nucleo board. nucleo-c031c6. 

As a matter of fact, I am using nucleo all the way, and not discovery as mentioned before.

 

The C031 may be carrying the gotcha from G0.

 

Rgds

 

Calvin


I have both Nucleo boards.

The Nucleo-C031C6 does not have that issue like the Nucleo-G071RB does, as it doesn't have the UCPDx peripheral.   

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source