Skip to main content
PB1
Associate III
Feb 7, 2020 10:02 PM UTC
Solved

Odd behavior in assembly busy wait cycle

I am preparing the labs for the undergraduate embedded systems course at the university where I work (the University of Milano-Bicocca in Italy). This year we will change the hardware and we will start using the STM32 Nucleo F767ZI boards. I am a total beginner, so please bear me. I am preparing the usual "blinky" example, so I started STM32CubeIDE, I created a fresh project, did not touch the default pinout configuration, and proudly wrote my first code for a Nucleo board ever:

/* main.c: */
...
int main(void)
{
 ...
 while (1)
 {
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0 | GPIO_PIN_7 | GPIO_PIN_14, GPIO_PIN_SET);
 PAUSE_CIRCA_ONE_SECOND;
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0 | GPIO_PIN_7 | GPIO_PIN_14, GPIO_PIN_RESET);
 PAUSE_CIRCA_ONE_SECOND;
 }
}
...

To spice the things up a bit I wrote the pause code in ARM inline assembly:

#define PAUSE_CIRCA_ONE_SECOND \
	asm volatile("mov r0, #0x4400000\n" \
				 "sub r0, r0, #1\n" \
				 "cmp r0, #0\n" \
				 "bne .-6" : : : "cc", "r0");

where I considered the 216MHz clock and I guessed that the CPU would execute approximately one instruction per clock cycle - hence 0x4400000. It turns out that the resulting behavior is almost as I would expect: the leds stay on for about one second, and this is great, but they stay off much longer, that is, for about 12 seconds. The interesting thing is that if I unroll the loop once:

while (1)
{
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0 | GPIO_PIN_7 | GPIO_PIN_14, GPIO_PIN_SET);
 PAUSE_CIRCA_ONE_SECOND;
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0 | GPIO_PIN_7 | GPIO_PIN_14, GPIO_PIN_RESET);
 PAUSE_CIRCA_ONE_SECOND;
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0 | GPIO_PIN_7 | GPIO_PIN_14, GPIO_PIN_SET);
 PAUSE_CIRCA_ONE_SECOND;
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0 | GPIO_PIN_7 | GPIO_PIN_14, GPIO_PIN_RESET);
 PAUSE_CIRCA_ONE_SECOND;
}

the leds always stay on for about one second, and stay off for about 12 seconds on the odd cycles (starting to count from 1) and for about 1 second on the even cycles. This behavior remains the same if I unroll the loop more than once. I would like to understand the reason of such a strange behavior.

I did some small investigations to exclude the most trivial causes. I don't think there is any difference between the many instances of the PAUSE_CIRCA_ONE_SECOND code: I disassembled the main() and compared them without finding any difference. Also, I used PC-relative offsets and cross-checked the branch target in the disassembled code to be sure that one instance does not jump into the other. The slow part is not the call to HAL_GPIO_WritePin: I debugged the code and setting/resetting the GPIO pins always takes a negligible amount of time when compared to PAUSE_CIRCA_ONE_SECOND.

Any explanation, any suggestion on how I can further investigate the causes, or any fix to the above code, is welcome.

Thank you in advance

Pietro Braione

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Feb 7, 2020 10:43 PM UTC

Nice!

  • get rid of as much of Cube/HAL as possible (as part of investigation, but also in school setting you IMO should avoid it) - mainly regular interrupts such as systick
  • disconnect debugger
  • switch off caches
  • run out of the TCM memory, run at low speeds where FLASH can run without waitstates
  • move the code up/down e.g. by adding NOPs, observing alignment of the jump target to 2^N boundaries

I'm not sure it's the best idea to start with a superscalar processor with speculative prefetch, a bunch of caches and a complex busmatrix. So, losing control is almost inevitable and hard to analyze. and you've been quite rightly hit by it in your very first attempt. I definitively would not like to have this as the main specimen for an undergraduate mcu course - except as an example how modern "embedded" departed far from the notion of "control".

Yes, I'm old fashioned and grumpy.

JW

13 replies

n2wx
Senior
Feb 7, 2020 10:32 PM UTC

If your part has instruction and data caches what happens if you turn them off and go back to the pre-unrolled version?

waclawek.jan
waclawek.janBest answer
Super User
Feb 7, 2020 10:43 PM UTC

Nice!

  • get rid of as much of Cube/HAL as possible (as part of investigation, but also in school setting you IMO should avoid it) - mainly regular interrupts such as systick
  • disconnect debugger
  • switch off caches
  • run out of the TCM memory, run at low speeds where FLASH can run without waitstates
  • move the code up/down e.g. by adding NOPs, observing alignment of the jump target to 2^N boundaries

I'm not sure it's the best idea to start with a superscalar processor with speculative prefetch, a bunch of caches and a complex busmatrix. So, losing control is almost inevitable and hard to analyze. and you've been quite rightly hit by it in your very first attempt. I definitively would not like to have this as the main specimen for an undergraduate mcu course - except as an example how modern "embedded" departed far from the notion of "control".

Yes, I'm old fashioned and grumpy.

JW

RMcCa
Senior II
Feb 8, 2020 12:05 AM UTC

Dunno, but I'm glad I'm not a student at your uni.

PB1
PB1Author
Associate III
Feb 8, 2020 9:29 AM UTC

LOL, sometimes I am also glad I am not.

Tesla DeLorean
Guru
Feb 8, 2020 1:08 AM UTC

Are you sure you've configured it to successfully run at 216 MHz, perhaps it is running at 16 MHz out of reset on the HSI

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PB1
PB1Author
Associate III
Feb 8, 2020 9:29 AM UTC

I did not touch the clock speed settings, and I reckon that if it were running slower the up-cycle would not last one second. But it is a possibility.

berendi
Principal
Feb 8, 2020 8:05 AM UTC

It might be an alignment issue, or the branch predictor is confused, maybe by the conditional branch followed by an unconditional one.

What happens if you move the last delay to the top of the loop like this?

In today's lesson we have seen why one should never use cpu loops as a delay. Next week, we will learn how to set up a hardware timer to generate proper timings.

n2wx
Senior
Feb 8, 2020 2:18 PM UTC

I think they still have their place during power up before everything is brought up, but not with HAL and maybe not with the opaque predictive caching this puppy may or may not do. It's frightening that the ref manual doesn't expose a way to turn off branch predictive caching if such a thing is implemented

berendi
Principal
Feb 8, 2020 2:45 PM UTC

If there were a way to turn off branch prediction, it'd rather belong to the programming manual. But there is no way.

PB1
PB1Author
Associate III
Feb 8, 2020 9:31 AM UTC

Thanks to everyone for your feedback. Of course the aim of this experiment is to say "never do this kind of things, use the fine timers instead". In my not so short teaching experience I have met the student who swapped integer variables with XOR to save 32 bits of temp - during a programming 101 course, on a machine with a giga of memory available, and after being told to write readable, rather than fast or tight, code. I therefore fully expect that some students will come to the conclusion that using a current-day ARM M7 as it were an 8051 is a good idea, and I want to prove them wrong as soon as possible before they hit the wall by themselves.

This said, I did some more experiments by disabling L1 instruction cache and fiddling with the size of the code (e.g., using a toggle and a single wait block in the loop), and I came to the conclusion that caching is most likely the cause. That's enough for me. Thanks to everyone for your suggestions and comments. And about the present day trend of using highly nondeterministic superscalar/pipelined/cached processors in embedded - and possibly safety-critical - settings, maybe I also am too old fashioned and grumpy so I will shut up.

waclawek.jan
Super User
Feb 8, 2020 10:27 AM UTC

> the aim of this experiment is to say "never do this kind of things, use the fine timers instead"

Never say never.

Loopdelay blinky is THE cornerstone when bringing up a new system.

> one should never use cpu loops as a delay

Never say never again...

Loopdelays are still useful in the - admittedly rare, but existing - cases, where short delays in the order of a few machine cycles are needed.

I'd say, "never" is good to be said in the first course (101 in the anglosaxon educational world), but later the refined truth should be taught, IMO.

JW

waclawek.jan
Super User
Feb 8, 2020 10:46 AM UTC

> I came to the conclusion that caching is most likely the cause.

I don't think so; I believe it's the speculative prefetch/branch prediction/branch address cache, or maybe even the dual issue.

Unfortunately, according to PM0253, branch prediction probably can't be switched off, and it does not mention BTAC at all so it's probably not implemented in the ST incarnations of Cortex-M7. Contrary to the Cortex-M7 TRM, PM0253 also states most of the "tweaking" bits of SCB_ACTLR register to be reserved, so these again are probably not implemented by ST. But - again contrary to the TRM - there appears to be a simple way to switch off the instruction cache, by clearing SCB_CCR.IC, so that's a simple thing and it would be nice if you'd try that.

JW

Piranha
Principal III
Feb 8, 2020 3:03 PM UTC

> about the present day trend of using highly nondeterministic superscalar/pipelined/cached processors in embedded - and possibly safety-critical - settings

If a device's ability to function correctly depends on exact CPU clock ticks in a complex MCU with multiple peripherals on multiple buses running simultaneously, then that is not a safety-critical device and IMHO not a reliable device at all. And it's true not only for Cortex-M7 but also for other more deterministic Cortex-M CPUs, because buses, flash memory accesses, interrupts, interrupt nesting and other features also introduce non-determinism.