Odd and Even CAN bus ID's FilterConfig
Hi, I am working with STM32F103 and configured CAN filter to receive ODD and EVEN ID's to FIFO0 and FIFO1 accordingly:
CAN_FilterTypeDef sFilterConfig;
sFilterConfig.SlaveStartFilterBank = 28;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
// odd IDs to FIFO0
sFilterConfig.FilterIdHigh = (0x00000001 << 5);
sFilterConfig.FilterIdLow = (0x00000000 << 5);
sFilterConfig.FilterMaskIdHigh = (0x00000001 << 5);
sFilterConfig.FilterMaskIdLow = (0x00000000 << 5);
if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
sFilterConfig.FilterBank = 1;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO1;
// even IDs to FIFO1
sFilterConfig.FilterIdHigh = (0x00000000 << 5);
sFilterConfig.FilterIdLow = (0x00000000 << 5);
sFilterConfig.FilterMaskIdHigh = (0x00000001 << 5);
sFilterConfig.FilterMaskIdLow = (0x00000000 << 5);
if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_CAN_Start(&hcan) != HAL_OK)
{
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan, CAN_IT_RX_FIFO1_MSG_PENDING) != HAL_OK)
{
Error_Handler();
}Its not that easy to understand STM32 filter mask and ID's. So is filter configured correctly to receive ODD and EVEN ID's to FIFO0 and FIFO1?
Also previously I was using only FIFO0 to catch all CAN bus ID's. Does splitting filters to ODD and EVEN ID's into FIFO0 and FIFO1 should give better performance and less overflow chance?