Skip to main content
Associate
January 8, 2025
Solved

OCTOSPI on STM32U5F9ZJT6Q

Dear, 

Can you confirm that OCTOSPI P2 is available only on WLCSP208 and TFBGA216 packages of this series? 

I wanted to use both OCTOSPI interfaces in LQFP144, but noticed that there is missing only OCTOSPIM_P2_IO3 line in it, so my conclusion is that LQFP144 supports only one OCTOSPI. Is that right? 

Thank you. 

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
February 27, 2026

Hello @Tesla DeLorean ;

 

A note is added in DS14395 Rev 4.

Screenshot 2026-02-27 152826.png

Screenshot 2026-02-27 152855.png
Also, this behavior is supported in STM32CubeMX 6.17.0 version.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

6 replies

KDJEM.1
ST Technical Moderator
January 8, 2025

Hello @Ivica,

 

According to the datasheet DS14395 Rev 2 Table 2. STM32U5Fxxx features and peripheral counts.

The STM32U5F9ZJ supports only one OCTOSPI interface. If you want to use two XSPIs interfaces with STM32U5F9ZJ package, I recommend you to use the OCTOSPI interface and HSPI interface, which are supported on STM32U5F9ZJ package.

KDJEM1_0-1736346535539.png

KDJEM1_1-1736346286456.png

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
January 8, 2025

Is there a way to mux/map via the SPIM provided one can escape OCTOSPIM_P2_NCS on exposed pins?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
KDJEM.1
ST Technical Moderator
January 8, 2025

Hello @Tesla DeLorean

 

Thank you for bringing this to our attention.

I will check internally is there any restriction to use the multiplexed mode on STM32U5F9ZJ? And there a way to mux/map via the SPIM provided to escape OCTOSPIM_P2_NCS?

Internal ticket number: 199853 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.