Skip to main content
Southbranch
Senior
Aug 8, 2024 3:53 PM UTC
Solved

OCTO SPI output impedance on H7-series

I have swapped from a custom PCB-board with a 6-layer stack using a STM32H725IGKB, to another custom board with a 4-layer stack using STM32H723ZGT6 (simpler package).

I am using an external OCTO SPI on both boards, but I have R/W errors with the 4-layer board.

Both boards are routed with 50 ohms impedance and uses 33 ohms series resistors for the OCTO SPI.

I am wondering if the output impedance is the same for these two H7-devices?

MHoll.2
MHoll.2Best answer
Senior III
Aug 9, 2024 12:38 PM UTC

Hi

LQFP package's are notoriously less performant than BGA's (longer bond wire), but this is probably not your problem.

Are PC2 and/or PC3 used for the OCTOSPI? This two pin's have special timing restriction on the STM32H723.

Martin

26 replies

LCE
Principal III
Aug 8, 2024 3:59 PM UTC

Have you checked the package pins?

I think concerning the packages, H723 is compatible with H733, and H725 with H735 - but I'm not 100% sure.

I just remember there was something that surprised me when I had to make that choice.

Concerning the output drivers - another guess: exactly the same.

PS: also check the alternate function numbers

Southbranch
Senior
Aug 9, 2024 7:45 AM UTC

Thanks,

Yes, pins are checked back and forth, but what do you mean with alternative function numbers?

@st_it, could you please confirm the output impedance is the same for these devices and that 33 ohms series resistors are recomended?

Thanks in advance

 

 

LCE
Principal III
Aug 9, 2024 10:51 AM UTC
	/* MCO */
	GPIO_InitStruct.Pin 		= LL_GPIO_PIN_8;
	GPIO_InitStruct.Mode 		= LL_GPIO_MODE_ALTERNATE;
	GPIO_InitStruct.Speed 		= LL_GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.OutputType 	= LL_GPIO_OUTPUT_PUSHPULL;
	GPIO_InitStruct.Pull 		= LL_GPIO_PULL_NO;
	GPIO_InitStruct.Alternate 	= LL_GPIO_AF_0;
	LL_GPIO_Init(GPIOA, &GPIO_InitStruct);

See ".Alternate = ...AF_0".

But it's probably the same between these types, so forget that...

Southbranch
Senior
Aug 9, 2024 12:12 PM UTC

Yes, thanks

They set as you layed out for both devices

MHoll.2
MHoll.2Best answer
Senior III
Aug 9, 2024 12:38 PM UTC

Hi

LQFP package's are notoriously less performant than BGA's (longer bond wire), but this is probably not your problem.

Are PC2 and/or PC3 used for the OCTOSPI? This two pin's have special timing restriction on the STM32H723.

Martin

Southbranch
Senior
Aug 10, 2024 7:01 AM UTC

Hi,

Yes I am using PC2_C and PC3_C - is there something I must take into consideration?

AScha.3
Super User
Aug 10, 2024 7:43 AM UTC

Hi,

>Yes I am using PC2_C and PC3_C - is there something I must take into consideration?

YES. The xx_C are not good to drive hi-speed signals :

ds:

AScha3_0-1723274755407.png

AScha3_1-1723275020957.png

So you have about 400 ohms source resistance here +

AScha3_2-1723275169084.png

AScha3_3-1723275345994.png

xx_C should be used only for ADC input ...

and should not drive more > 1mA , otherwise you might kill it . (I did - so i know - with just the clock to a TFT on a xx_C pin. Testing TFT with 4MHz clock was ok, but then i switched to 16MHz - 1 screen written, then pin died. )

So dont use these pins for hi-speed signals - they cannot drive it. If you cannot change it now, try with 

ed : low speed setting (400 ohm in series ! ) , just to verify your design is working. (maybe 2 MHz clock...)

 

If you feel a post has answered your question, please click on " Best Answer ".
Tesla DeLorean
Guru
Aug 9, 2024 12:40 PM UTC

Make sure the "Compensation Cell" is enabled. You can also back off the Speed setting on short traces.

Some memories also allow the load or drive to be adjusted.

Any difference in the chip and bus clocking between boards?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Southbranch
Senior
Aug 10, 2024 7:11 AM UTC

Thanks Tesla,

  • I have tried enable the compensation cell
  • I lowered GPIO speed from "very high" to "high" and "medium" - if that is what you meant?
  • I guess the load (or impedance) could be adjusted via the memory's register, but have not tried it yet, should be default 50 ohm and all traces are routed in 50 ohm.
  • Exactly the same bus set-up and clocking for both boards

I discovered that I used 30 ohms (5% tolerance) series resistors rather than 33 ohms due to lack in inventory but is a small margin and it should probably not be the cause. I am out of ideas and I begin thinking there perhaps could been some issue with the PCB stack-up during manufacturering.

 

Southbranch
Senior
Aug 12, 2024 8:48 AM UTC

Thanks,

@st_it, could you please provide a comment on this (impedance + PC2/PC3 pins) before I start re-design my PCB?

AScha.3
Super User
Aug 12, 2024 7:08 PM UTC

Hi,

Just looking at ds, pin list, at pins PC2+3 :

If "standard" pin, standard timing - as expected.

If something other, like _a -- other timing, need look at details for this kind of pin.

If you feel a post has answered your question, please click on " Best Answer ".
Southbranch
Senior
Aug 13, 2024 7:09 AM UTC

Thank again,

Could you please elaborate a bit.

I have checked RM0468 but I can’t find anything explicitly stating that PC2_C/PC3_C could not be used for high speed communication.

LCE
Principal III
Aug 13, 2024 10:41 AM UTC

Check the datasheet not the RM, search for "PC2".

LCE_0-1723545340377.png

Datasheet of H733, should be the same for H723/H725.

See note 4.

Even worse, see again note 4 for HyperBus, max freq with PC2 is 47 MHz:

LCE_1-1723545511166.png

Dear ST, this should not be in smallest print in some footnotes, but bold and BIG in each mentioning of every use outside of analog input.

There was no CubeMX warning?

Southbranch
Senior
Aug 13, 2024 4:07 PM UTC

Many thanks LCE for providing this info.

Please ST, perhaps you could also comment on this before I start re-route my PCB-traces?

BarryWhit
Lead
Aug 13, 2024 5:01 PM UTC
"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
Southbranch
Senior
Aug 14, 2024 7:43 AM UTC

Thanks for pointing me to previous threads,

The first was from 2021 but was indeed covering the PC_2/PC_3 issues. Now, it seems the fastest action to get onwards would be for me to re-route traces with other GPIOs to rule out this potential cause.

LCE
Principal III
Aug 14, 2024 8:27 AM UTC

Memory-mapped mode doesn't even work with a clock rate of 20 MHz (or anything else below the 47 MHz mentioned in the datasheet) ?

The ringing you see on the scope might come from your scope measurement itself, always use a spring tip for GND, not the usual 10cm or so GND clip.

Southbranch
Senior
Aug 14, 2024 10:18 AM UTC

Memory mapped mode works fine with OCTO SPI freq. set to 166 MHz (max for the chip) on the 6-layer board.

On the 4-layer board R/W does not seem to work even how low I set the freq.

AScha.3
Super User
Aug 14, 2024 2:59 PM UTC

Try at very low speed, 4 or even 1 MHz, to prove your design, but check with scope, the _C pins still working at all ( as I said, I killed one just by using at 16 Mbit - then it never worked again ! ). So maybe you already have a dead pin, then cannot use it to prove the design.

 

 

 

If you feel a post has answered your question, please click on " Best Answer ".
Southbranch
Senior
Aug 15, 2024 7:05 AM UTC

Thank you all for contributing with good ideas and advices, highly appreciated :smiling_face_with_smiling_eyes:

I'll park this thread now and will go ahead with a new PCB-design without using PC2_C/PC3_C.

Southbranch
Senior
Aug 29, 2024 10:46 AM UTC

Problem solved!

It turned out to be the PC2_C/PC3_C pins that caused the faulty communication. I just received a new PCB-version of our custom board and it all works fine now using another pin assignments.

Many, many thanks for pointing this out :grinning_face: