Question
Octo-SPI memory-mapped mode speed for H735
Hi,
We are using the OCTOSPI2 on a H735 in memory map mode.
We are copying 32 bits values one by one, from the internal RAM to the Octo memory.
We transfer around 5000 x 32 bits in 2ms which is around 10MB/s.
I think, it is a bit slow. What is the maximum speed we could achieve ?
Perhaps we have done a mistake in the different clocks or GPIOs settings ?
All advice is welcomed !
Have a nice day and week-end !
Olivier