Skip to main content
Senior
October 11, 2024
Solved

NVIC TIM / I2C DMA Priority issue

  • October 11, 2024
  • 2 replies
  • 1265 views

Hello Community, 

I am using a STM32F411, 

2 timer with global interrupt and preemption priority of 0 are executing a timing critical process to bitbang a GPIO port.

4uS timer period

And 

a I2C DMA process to update a SSD1306 screen I2C and DMA interrupt have a preemption priority of 14

I am having an issue with the timer bitbang when I sent a message to update the screen. 

I thought that lower interrupt priority with take the lead and it seems that it is not the case

Do I miss something ?

Vincent

 

 

 

This topic has been closed for replies.
Best answer by waclawek.jan

Make sure the problem is indeed caused by the priorities, e.g. by toggling pins in the ISRs and checking on oscilloscope for overlap (or lack thereof).

If you've confirmed it, read out and check/post content of NVIC registers (namely NVIC_IPR[]), and SCB_AIRCR to check the PRIGROUP field.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
October 11, 2024

Make sure the problem is indeed caused by the priorities, e.g. by toggling pins in the ISRs and checking on oscilloscope for overlap (or lack thereof).

If you've confirmed it, read out and check/post content of NVIC registers (namely NVIC_IPR[]), and SCB_AIRCR to check the PRIGROUP field.

JW

vbessonAuthor
Senior
October 11, 2024

the issue was a sub priority problem. now fixed

thanks

Vincent