Skip to main content
optifier
Associate II
March 27, 2013
Question

Number of ADC channels in STM32F207Zx?

Posted on March 27, 2013 at 21:57

Hi,

Trying to get my head around how many ADC channels that are available in STM32F207Zx chip.

Datasheet p14 Table3 claim ''Number of channels = 24''.

Also on p.1 ''ADC with up to 24 channels''.

OTOH, Reference manual p.204 says ''19 multiplexed channels allow it to measure signals from 16 external sources''.

I can count to 24 pins on 144-pin chip that have ADC available. But none of the pins go beyond ADCxxx/IN15.

Is this some sort of marketing trick to claim 24 channels in Datasheet?

Or is there some multiplexing scheme that allow us to use 2 separate external sources connected to i.e. AD12/IN15 and ADC3/IN15 if we catch the result from first conversion before starting a second one with same INxx number?

One of the major reasons we've looked into using STM32F207Zx chip was the large number of ADC channels advertised in Datasheet.

Please enlighten me..

/Richard

#adc-channels
    This topic has been closed for replies.

    7 replies

    ezendam
    Visitor II
    March 27, 2013
    Posted on March 27, 2013 at 22:09

    I am working with a stm32f4xx which has also 16 extexnal channels. But the adc can have up to 19 signals. 3 of them are internal signals like temp-sensor, vbat, etc. Can this be the case in your situation?

    optifier
    optifierAuthor
    Associate II
    March 27, 2013
    Posted on March 27, 2013 at 22:19

    No, I'm aware of the 3 internal channels that make a total of 19 channels stated in Reference manual.

    raptorhal2
    Lead
    March 27, 2013
    Posted on March 27, 2013 at 22:51

    Or is there some multiplexing scheme that allow us to use 2 separate external sources connected to i.e. AD12/IN15 and ADC3/IN15 if we catch the result from first conversion before starting a second one with same INxx number?

    There are 3 ADCs, and some input channels can be connected to any one of 2 or 3 of these at a given time. The pinout definition defines which are which, e.g, ADC123_INx can be connected to one of the three, ADC12_INx to ADC1 or ADC2. Packages with a high pin count have an additional 8 channels connected to ADC3 only, and that provides for 24 external channels.

    Clear ?

    Cheers, Hal

    raptorhal2
    Lead
    March 27, 2013
    Posted on March 27, 2013 at 22:59

    And if you are really channel hungry, the F3 series has 4 ADCs with something like 38 external channels.

    Cheers, Hal

    optifier
    optifierAuthor
    Associate II
    March 27, 2013
    Posted on March 28, 2013 at 00:57

    Hello Hal,

    Well, clear is maybe not the correct word for my state of mind.

    If I understand correct you're saying:

    There ARE 24 ADC inputs on the chip and i.e. ADC12/IN15 and ADC3/IN15 can both be active at same time, not interfering with each other.

    That is, we can connect 2 separate sources and use ADC1(or ADC2) to read ADC12/IN15 and ADC3 to read ADC3/IN15 and expect two different results not related to / wiping out results of each other.

    And that Reference manual stating that 16 external sources can be connected are true for smaller pin-count devices, but not quite true for devices with ADC3.

    So far we'll be happy with 24 channels but good to know that there is a real monster out there with 38 channels.

    /Richard

    Tesla DeLorean
    Guru
    March 28, 2013
    Posted on March 28, 2013 at 01:42

    That is, we can connect 2 separate sources and use ADC1(or ADC2) to read ADC12/IN15 and ADC3 to read ADC3/IN15 and expect two different results not related to / wiping out results of each other.

    Indeed, the different ADCx units can scan through a different assortment of pins. You have to use DMA to store the results from each ADC conversion when dealing with multiple channels on a single unit.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    optifier
    optifierAuthor
    Associate II
    March 28, 2013
    Posted on March 28, 2013 at 09:48

    Now I feel reassured.

    Thanks to all that helped to set my mind at ease again..

    /Richard