Skip to main content
stm32f4
Associate III
May 28, 2018 3:21 PM UTC
Solved

NUCLEOL476RG read battery level using ADC.

Posted on May 28, 2018 at 17:21

Hello ST All.

I have a NUCLEOL476RG and i have some troubles trying to read a battery level using ADC.

I made a voltage divider partitor to get 3.3V starting from 14.1V.

1)  using 162K resistor + 50K resistor the adc read 2.9v

2) using 68.8k + 20.78k the adc read 2.6v.

Using multimeter on partitor in both read 3.20v .

If i read 3.3 from Nucleo (CN7  pin 2 or 4) adc read correctly.

please, Anyone may helm me with hints?

Regards,

Carmelo

    This topic has been closed for replies.
    S.Ma
    S.MaBest answer
    Principal
    May 28, 2018 4:04 PM UTC
    Posted on May 28, 2018 at 18:04

    ADC input is high impedence. Then ADC sample the voltage by connecting a RC to the ADC input pin for a while, then disconnecting the input pin, and convert. When connecting the RC, the cap maybe discharged...

    The input impedence should be small (ideally a supply voltage), and here it is very resistive, the RC curve slows down and is cut before reaching the asymptotic ideal voltage.

    ==> If this situation is correct, increasing the sample time to maximum will yield a value closer to the expected one.

    ==> If the required sample time shall be higher than possible, you could stop the ADC clock during sampling phase to 'freeze the time'.

    ==> Alternatively, put a decoupling cap to ground (10uF?) at the ADC sampling point. Battery level changes slowly so the response time of the divider maynot be critical...

    3 replies

    S.Ma
    S.MaBest answer
    Principal
    May 28, 2018 4:04 PM UTC
    Posted on May 28, 2018 at 18:04

    ADC input is high impedence. Then ADC sample the voltage by connecting a RC to the ADC input pin for a while, then disconnecting the input pin, and convert. When connecting the RC, the cap maybe discharged...

    The input impedence should be small (ideally a supply voltage), and here it is very resistive, the RC curve slows down and is cut before reaching the asymptotic ideal voltage.

    ==> If this situation is correct, increasing the sample time to maximum will yield a value closer to the expected one.

    ==> If the required sample time shall be higher than possible, you could stop the ADC clock during sampling phase to 'freeze the time'.

    ==> Alternatively, put a decoupling cap to ground (10uF?) at the ADC sampling point. Battery level changes slowly so the response time of the divider maynot be critical...

    T J
    Senior III
    May 29, 2018 2:36 AM UTC
    Posted on May 29, 2018 at 02:36

    decoupling cap should be closer to 1uF or even 0.1uF,

    your problem is the high impedance.

    if you require a fast response, then you should use an external OpAmp to drive the pin with low impedance.

    this will give you a much faster changing voltage on the pin from the source and a rapid read capability.