Skip to main content
yang hong
Associate III
Apr 30, 2024 3:30 PM UTC
Question

nucleof439 lwip

I am using nucleof439 to work Lwip, however, when I configure the project in stm32cubeide, I generate the code, and comply the project. It is fine, I also can ping the device, however, when I reenter ping command from windows cmd, the device is blocked, anybody know why?

 

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
Apr 30, 2024 3:44 PM UTC

@yang hong wrote:

 when I reenter ping command from windows cmd, the device is blocked


What do you mean by that?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
Apr 30, 2024 5:04 PM UTC

Hello,

Do you mean that the ping success only once and the second ping has no response?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.