Question
Nucleo64 - default blinky description
UM1724 rev.12, in chapter 5.1 Getting started in description of the default blinky program which comes preprogrammed with the board, says:
5. Observe the blinking frequency of the three LEDs LD1 to LD3, by clicking on the button
B1.
What?
LD1 is STLink's LED, the application mcu has no influence on it. LD3 is a power LED, indicating presence of +5V from whatever source.
This sentence should say, Observe the blinking of LD2 changing between three frequencies, by clicking on the the button B1.
JW