Skip to main content
JNoon.1
Associate III
September 11, 2023
Solved

Nucleo STM32U575ZI-Q low level USART receiving help

  • September 11, 2023
  • 4 replies
  • 3048 views

Hi all,

I am using the Nucleo STM32U575ZI-Q and have been trying to get low level USART with DMA working. Transmitting data works fine as I can see the data using a logic analyser but when I try to receive data either from another Nucleo or putting the wire from Tx to Rx I get nothing.

I have a Asynchronous USART with DMA channels for both Tx and Rx. 

In MX_USART1_UART_Init() I enable:

 

 LL_DMA_EnableIT_HT(GPDMA1, LL_DMA_CHANNEL_10);
 LL_DMA_EnableIT_TC(GPDMA1, LL_DMA_CHANNEL_10);

 LL_DMA_EnableIT_TC(GPDMA1, LL_DMA_CHANNEL_11);

 LL_USART_EnableIT_IDLE(USART1);

 

In my other init function for my code I set the DestAddress, BlkDataLength and also enable the channel:

 

 LL_DMA_SetDestAddress(pDMATypedef, LL_DMA_CHANNEL_10, (uint32_t)RXBuffer);
 LL_DMA_SetBlkDataLength(pDMATypedef, LL_DMA_CHANNEL_10, mARRAY_LEN(RXBuffer));

 LL_DMA_EnableChannel(pDMATypedef, LL_DMA_CHANNEL_10);

 

In my Rx DMA interrupt I call a function which calls another function which will check if there is any data in the buffer. This checking function also gets called from the USART interrupt. 

 

My problem is when it comes to check the data in the buffer there is nothing:

 

uint32_t u32Pos = sizeof(RXBuffer) - LL_DMA_GetBlkDataLength(pDMATypedef, LL_DMA_CHANNEL_10);

 

This function does not get called from the Rx DMA interrupt but from the USART interrupt.

Is there anything I have missed or have not done correctly?

If there is any other information needed please ask! 

Many thanks!

This topic has been closed for replies.
Best answer by JNoon.1

Hi @Foued_KH 

I have fixed my problem thanks!

In MX_USART1_UART_Init in main.c, cube was not generating 2 function calls which I seemingly need. 

I had to add:

 

NodeConfig.SrcAddress = LL_USART_DMA_GetRegAddr(USART1, LL_USART_DMA_REG_DATA_RECEIVE);

 

To the auto generated code, as I cannot add this to the user defined area.

But I also had to add these two calls to my user defined area:

 

 LL_DMA_ConfigLinkUpdate(GPDMA1, LL_DMA_CHANNEL_0,
 (LL_DMA_UPDATE_CTR1 | LL_DMA_UPDATE_CTR2 | LL_DMA_UPDATE_CBR1 | LL_DMA_UPDATE_CSAR
 | LL_DMA_UPDATE_CDAR | LL_DMA_UPDATE_CTR3 | LL_DMA_UPDATE_CBR2 | LL_DMA_UPDATE_CLLR),
 (uint32_t)&Node_GPDMA1_Channel0);

 LL_DMA_EnableChannel(GPDMA1, LL_DMA_CHANNEL_0);

 

 The LL_DMA_ConfigLinkUpdate call should probably be auto generated but it is not.

And as for LL_DMA_EnableChannel, I do call this in another part of my code as part of initialisation but for some reason it needs to be called here as well.

Thanks.

4 replies

Foued_KH
ST Employee
September 11, 2023

Hello  @JNoon.1 , 

I suggest you to check the available examples : STM32CubeU5/Projects/NUCLEO-U575ZI-Q/Examples_LL/USART at main · STMicroelectronics/STM32CubeU5 · GitHub

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JNoon.1
JNoon.1Author
Associate III
September 11, 2023

Hi @Foued_KH, 

Thank you for your reply. Unfortunately I have been looking at the examples and this one (https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx/blob/main/projects/usart_rx_idle_line_irq_ringbuff_tx_loopback_U5/Src/main.c) but neither seem to help me in this situation. I have been looking through the examples and I am not seeing anything in particular that is wrong.

Google isn't the biggest help either as there are not many LL USART examples out there for the U5 series.

Thanks.

Foued_KH
ST Employee
September 11, 2023

you can refer to this source file ( from STM32L5 CubeFW) it may help you !

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.