Skip to main content
AKuma.33
Associate II
November 18, 2021
Question

NUCLEO-L4P5ZG to NRF52-DK SPI not working, but works with NUCLEO-F446RE.

  • November 18, 2021
  • 3 replies
  • 1057 views

Hi,

I am trying to use Nucleo-l4p5 as SPI Master and NRF52 as slave.

Issue : nrf is reading wrong and partial data and when I am connecting GND of both boards, it stops working.

Solutions tried so far:

  1. I have tried the same code with Nculeo-F446RE and NRF52-DK:
    1. It is sending wrong and partial data, GND not common between boards.
    2. It works as expected with GND common.
  2. I have tried Nucleo-l4p5(Master) to Nucleo-l4p5(Slave), with GND connected. It works as expected.
  3. I have tried powering One board with another, but again freezing issue.
  4. I have tried lowering the master clock.

// ST master code
 while (1)
 {
 
	 if (count%2 == 1)
	 {
	 	 memset(buffer1, buffer1, 6);
		 HAL_GPIO_WritePin(cs_port, cs_pin, GPIO_PIN_RESET);
		 HAL_Delay(10);
		 HAL_SPI_Transmit(&hspi3, &buffer1, 6, 100);
		 HAL_Delay(10);
		 HAL_GPIO_WritePin(cs_port, cs_pin, GPIO_PIN_SET);
	 }
	 else
	 {
		 memset(buffer1, buffer1, 6);
		 HAL_GPIO_WritePin(cs_port, cs_pin, GPIO_PIN_RESET);
		 HAL_Delay(10);
		 HAL_SPI_Transmit(&hspi3, &buffer1, 6, 100);
		 HAL_Delay(10);
		 HAL_GPIO_WritePin(cs_port, cs_pin, GPIO_PIN_SET);
	 }
	 count++;
	 HAL_Delay(1000);

Clock is configured for PCLK1(60) and PCLK2(120)

This is the configuration:

static void MX_SPI3_Init(void)
{
 
 /* USER CODE BEGIN SPI3_Init 0 */
 
 /* USER CODE END SPI3_Init 0 */
 
 /* USER CODE BEGIN SPI3_Init 1 */
 
 /* USER CODE END SPI3_Init 1 */
 /* SPI3 parameter configuration*/
 hspi3.Instance = SPI3;
 hspi3.Init.Mode = SPI_MODE_MASTER;
 hspi3.Init.Direction = SPI_DIRECTION_2LINES;
 hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi3.Init.NSS = SPI_NSS_SOFT;
 hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
 hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi3.Init.CRCPolynomial = 7;
 hspi3.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi3.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 if (HAL_SPI_Init(&hspi3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI3_Init 2 */
 
 /* USER CODE END SPI3_Init 2 */
 
}

This topic has been closed for replies.

3 replies

TDK
November 18, 2021

GND needs to be common between the boards so they both have the same reference voltage.

What data do you receive and what data are you expecting instead?

> memset(buffer1, buffer1, 6);

What is this supposed to do?

"If you feel a post has answered your question, please click ""Accept as Solution""."
AKuma.33
AKuma.33Author
Associate II
November 19, 2021

Sorry for the typo, this is what I am sending:

 while (1)
 {
 
	 if (count%2 == 1)
	 {
	 	 memset(buffer1, 68, 6);
		 HAL_GPIO_WritePin(cs_port, cs_pin, GPIO_PIN_RESET);
		 HAL_Delay(10);
		 HAL_SPI_Transmit(&hspi3, &buffer1, 6, 100);
		 HAL_Delay(10);
		 HAL_GPIO_WritePin(cs_port, cs_pin, GPIO_PIN_SET);
	 }
	 else
	 {
		 memset(buffer1, 65, 6);
		 HAL_GPIO_WritePin(cs_port, cs_pin, GPIO_PIN_RESET);
		 HAL_Delay(10);
		 HAL_SPI_Transmit(&hspi3, &buffer1, 6, 100);
		 HAL_Delay(10);
		 HAL_GPIO_WritePin(cs_port, cs_pin, GPIO_PIN_SET);
	 }
	 count++;
	 HAL_Delay(1000);
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }

This is what I get at Receiving side:

<info> app: Transfer completed. Received: DDD
<info> app: Transfer completed. Received: ADD
<info> app: Transfer completed. Received: AAA
<info> app: Transfer completed. Received: AAAAA
<info> app: Transfer completed. Received: AAAAAA
<info> app: Transfer completed. Received: DDAAAA
<info> app: Transfer completed. Received: DDDDDA

The issue is I am not able to check operation while GND common, as I stop getting data at all.

Do 144-pin Nucleo boards have Isolated supplies or something?

TDK
November 19, 2021

If connecting GND breaks things, there is a hardware issue somewhere. Since the SPI signal is low a 0V and high at 3.3V, you need to ensure both parties have the save 0V reference. I do not believe any Nucleo boards have isolated supplies. Easy enough to check with a multimeter.

How do you know the issue isn't on the slave side? Can you put a logic analyzer on the lines to inspect data coming out?

I would wager your (new) code is correct and the issue is elsewhere.

"If you feel a post has answered your question, please click ""Accept as Solution""."