Skip to main content
Qye
Associate II
December 12, 2023
Question

Nucleo L476RG at 1.8V

  • December 12, 2023
  • 3 replies
  • 7696 views

I want to run a Nucleo L476RG at 1.8V at first glance it looks possible with a few caveats.

according to the schematic (C03)
https://www.st.com/en/evaluation-tools/nucleo-l476rg.html#cad-resources

There are two regulators I need to be concerned with

U4 which provides Vdd to the Main CPU is an LD39050PU33R (3.3V)
Unfortunately, this part does not come in a 1.8V version

I can either choose something like LD112PV18R (pin compatible 1.8V)
Or put in a LD39050PUR with an adjustment network spliced on.

 

The second is U1 used to create 3V3_ST_LINK an LD3985M33R (3.3V)

There is an alternate part LD3985M18R I can use to get 1.8V


One concern I have is the ST-LINK CPU
U2 STM32F103CBT6

The Vdd range specified in 2.0 to 3.6 volts.

I will try running it at 1.8V but might have to detach the ST Link
If I do, I will set the main board to be able to switch between 1.8V or 3.3V


The other concern is the USB ST-Link
I assume I cannot use this as there is no provision for the voltage conversion of USB_DM or USB_DP or USB_RENUMn

Or I can rig up a TXS0108E to shift voltages (except 5V) so I can still use the USB.


Have I missed anything?

This topic has been closed for replies.

3 replies

Qye
QyeAuthor
Associate II
December 12, 2023

And last one

ST Employee
December 12, 2023

Hi All,

 

Your community question has been routed to our online support center for support from our team.

 

Regards,
Jake

ST Support