Associate II
August 11, 2015
Question
Nucleo-L053R8
- August 11, 2015
- 9 replies
- 1490 views
Posted on August 11, 2015 at 12:00
Hello,
I'm using nucleo-l053r8 for my project. I have to make a data logger application with a sensor. Here i have developed my code in mbed tool. I also store the values in SD card. Now my task is to make my own custom board.After seeing schematics i realised that ST link has more components than controller. How can i make my custom board?. What are the components can i ignore.How can i dump the code in to the custom board. ( should i use ST link ).Once code flash in to the controller, since then it has to work on that code parmanently.