Skip to main content
Associate
September 18, 2023
Solved

Nucleo-H755ZI-Q not detected by usb

Hi there

I bought two Nucleo-H755ZI-Q (NUH755ZIQ$AT3) boards.
Non of them show up as USB devices on either of my computers.

I have tried connecting through the IDE 1.13.1; STLinkUpgrade  3.12.3 and the newest cubeprogrammer. neither can find the device.

I suspected driver issue and reinstalled the en.stsw-link009 driver
Still no luck; also the devices are not shown as "unknown" there is no reaction at all from the PC when i plug and unplug the device.

The MCU is running the preprogrammed program that switches between LD1,2 and 3 when user button is pressed. but except from that; nothing is working.
They also do not show up as 

This topic has been closed for replies.
TDK
TDKBest answer
September 18, 2023

Are you using the CN1 USB connector?

Perhaps try a different USB cable, could be using a power-only cable.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

Issamos
Super User
September 18, 2023

Hello @JOKH 

Can you try to connect under reset using Cube Programmer.

Best regards.

II

TDK
TDKBest answer
September 18, 2023

Are you using the CN1 USB connector?

Perhaps try a different USB cable, could be using a power-only cable.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JOKHAuthor
Associate
September 19, 2023

I did use the CN1 but the two cables I tried were apparently power-only cables.
I guess third time really is the charm.

Thank you for your response.