Skip to main content
Associate II
Apr 17, 2024 3:08 AM UTC
Question

Nucleo H723ZG SPI1 interrupt not reading FIFO ( register level programming - no HAL)

Using NUCLEO H723ZG & STM32 CUBE IDE

Trying to send two 32bit data (0xA & 0xB) via spi1 (only two 32bit words per data pkg)

NOTE- set up nucleo to close loop back & connected MISO & MOSI / clk=~2.182MHz

SPI1 set to 32bit w/ interrupt

I load 0xA & 0xB in FIFO & then SPI_CR1_CSTART

The chip goes into SPI1_IRQHandler(void)

1)However, though I see the value of RXDR sequence thru 0xA&0XB in debug SFR display,

but I always read as 0 in program

2) The prog seems to enter the IRQ handler only once

I was wondering if someone can comment

-spent a lot of time reading thru the RM0468 ref manual SPI section-I must have missed something!

 

Here is the code snippet (this is the only peripheral i am using)

 

main()

{

...//set up generated by IDE here

 

//set up SPI1

NVIC_EnableIRQ(SPI1_IRQn);//enable SPI1 global interrupt

SPI1->CR1 &= ~SPI_CR1_SPE;//disable spi1

SPI1->CR2 = 0x2;//TSIZE = two words to transmit

SPI1->CFG1 = SPI1->CFG1 | 0x00000030;//(FIFO threshold=3)

SPI1->IER |= SPI_IER_RXPIE;//enable RXPIE

SPI1->CR1 |= SPI_CR1_SPE;//enable spi1

SPIBusy=0;

while (1)

{

if(SPIBusy==0)

{

SPIBusy=1;//reset inside SPI1_IRQHandler(void)

SPI1->TXDR = 0xA;//first word into FIFO

SPI1->TXDR = 0xB;//second word into FIFO

SPI1->CR1=SPI1->CR1 | SPI_CR1_CSTART; //start transfer now

}

/* USER CODE END WHILE */

 

/* USER CODE BEGIN 3 */

}

/* USER CODE END 3 */

}

 

here is the IRQ handler

void SPI1_IRQHandler(void)

{

/* USER CODE BEGIN SPI1_IRQn 0 */

 

/* USER CODE END SPI1_IRQn 0 */

//HAL_SPI_IRQHandler(&hspi1);

/* USER CODE BEGIN SPI1_IRQn 1 */

 

SPIBusy = 0;

SPIReceivedData1 = SPI1->RXDR;//SPIReceivedData1=0 -expecting 0xA

SPIReceivedData2 = SPI1->RXDR;//SPIReceivedData2=0 -expecting 0xB

 

/* USER CODE END SPI1_IRQn 1 */

}

This topic has been closed for replies.