Skip to main content
John F.
Associate III
April 4, 2018
Question

NUCLEO-F767ZI Demo Software

  • April 4, 2018
  • 3 replies
  • 1234 views

Posted on April 04, 2018 at 16:58

Where can I find the source of the demo software which is already loaded on a 'fresh from the box' NUCLEO-F767ZI please. I searched the forum and looked on the ST nucleo web pages already.

Thanks - John F.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
April 4, 2018
Posted on April 04, 2018 at 17:29

I might have a .BIN or .HEX laying around somewhere.

Not convinced this is the code in question, but are other examples

STM32Cube_FW_F7_V1.9.0\Projects\STM32F767ZI-Nucleo\Demonstrations\readme.txt

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Technical Moderator
April 4, 2018
Posted on April 04, 2018 at 17:31

Hello

FitzGerald.John

,

There is aDemonstration firmware within STM32CubeF7 that can be plugged on a NUCLEO-F767ZI board and helps you to discover STM32 Cortex-M devices :

STM32Cube_FW_F7_V1.0\Projects\STM32F767ZI-Nucleo\Demonstrations

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
John F.
John F.Author
Associate III
April 5, 2018
Posted on April 05, 2018 at 09:00

Thanks for the quick replies Clive and Imen. 'Not convinced this is the code in question' ... I was looking for the source of the demo described in the Nucleo 'Quick start UM1974 10/82 DocID028599 Rev 7' where ...

To power the board connect the STM32 Nucleo-144 board to a PC with a USB cable ‘Type-A to Micro-B’ through the USB connector CN1 on the ST-LINK. As a result, the green LED LD6 (PWR) and LD4 (COM) light up and the red LED LD3 blinks.

4. Press button B1 (left button).

5. Observe the blinking frequency of the three LEDs LD1 to LD3 changes, by clicking on the button B1.

It's not really important. I was just going to start with the demo. I'll look at the other demo's and examples and work from there.

Thanks again. John F.