Skip to main content
Jos Poelmans
Associate II
April 25, 2017
Question

nucleo-F767ZI CAN bug

  • April 25, 2017
  • 0 replies
  • 513 views
Posted on April 25, 2017 at 14:10

I use CAN1 and CAN3 on the nucleo board and generate CAN code with stmCube version 4.20.

After automatic init CAN1 and CAN3 I deinit the can and then I try to init CAN1 again.

CAN1 is not working.

I'm looking in the can.c code and found ther I think a bug.

I have change the following in the code.

void

HAL_CAN_MspDeInit(

CAN_HandleTypeDef

* canHandle)

{

if

(canHandle->

Instance

==CAN1)

{

/* USER CODE BEGIN CAN1_MspDeInit 0 */

//*******************************************************

//*******************************************************

HAL_RCC_CAN1_CLK_ENABLED--;

// MY CHANGE in the code

//*******************************************************

//*******************************************************

/* USER CODE END CAN1_MspDeInit 0 */

/* Peripheral clock disable */

__HAL_RCC_CAN1_CLK_DISABLE();

/**CAN1 GPIO Configuration

PD0 ------> CAN1_RX

PD1 ------> CAN1_TX

*/

HAL_GPIO_DeInit

(GPIOD, CAN_1_RX_Pin|CAN_1_TX_Pin);

/* Peripheral interrupt

Deinit

*/

HAL_NVIC_DisableIRQ

(

CAN1_TX_IRQn

);

HAL_NVIC_DisableIRQ

(

CAN1_RX0_IRQn

);

HAL_NVIC_DisableIRQ

(

CAN1_RX1_IRQn

);

HAL_NVIC_DisableIRQ

(

CAN1_SCE_IRQn

);

/* USER CODE BEGIN CAN1_MspDeInit 1 */

/* USER CODE END CAN1_MspDeInit 1 */

}

else if

(canHandle->

Instance

==CAN3)

{

/* USER CODE BEGIN CAN3_MspDeInit 0 */

/* USER CODE END CAN3_MspDeInit 0 */

/* Peripheral clock disable */

__HAL_RCC_CAN3_CLK_DISABLE();

__HAL_RCC_CAN2_CLK_DISABLE();

HAL_RCC_CAN1_CLK_ENABLED--;

if

(HAL_RCC_CAN1_CLK_ENABLED==0){

__HAL_RCC_CAN1_CLK_DISABLE();

}

/**CAN3 GPIO Configuration

PA8 ------> CAN3_RX

PB4 ------> CAN3_TX

*/

HAL_GPIO_DeInit

(CAN_2_RX_GPIO_Port, CAN_2_RX_Pin);

HAL_GPIO_DeInit

(CAN_2_TX_GPIO_Port, CAN_2_TX_Pin);

/* Peripheral interrupt

Deinit

*/

HAL_NVIC_DisableIRQ

(

CAN3_TX_IRQn

);

HAL_NVIC_DisableIRQ

(

CAN3_RX0_IRQn

);

HAL_NVIC_DisableIRQ

(

CAN3_RX1_IRQn

);

HAL_NVIC_DisableIRQ

(

CAN3_SCE_IRQn

);

/* USER CODE BEGIN CAN3_MspDeInit 1 */

/* USER CODE END CAN3_MspDeInit 1 */

}

}

After that it is working. but I do not understand why CAN2 and CAN1 clock is needed

for CAN3. I hope in next cube version the code is  corrected.

    This topic has been closed for replies.