Skip to main content
BSchm.0
Associate III
Jan 24, 2019 11:12 AM UTC
Question

NUCLEO-F767ZI Arduino subset has wrong spacing

I tried to plug a shield arduino RS485 shield that fits on NUCLO-F401RE without any chance because of wrong spacing :thumbs_down:

This topic has been closed for replies.

2 replies

MNapi
Senior II
Jan 24, 2019 11:52 AM UTC

those pins are spaced I believe 2.5 mm which is standard for the connectors. Use jumper connectors. for example the arduino mcufriend tft display plugs in without problem. which is very nice combo. Except the fact I couldn't not find any libraries to light it up.

Uwe Bonnes
Chief
Jan 24, 2019 11:52 AM UTC

Are you sure you tried to plug it in the right connectors with the right orientation? We already used arduino shield on the NUCLEO-F767ZI with no problem.