Nucleo-F410RB DAC hardwired to a (green) LED ?
Friendly greetings !
i had found, ordered and canceled the board with the perfect MCU.
- M4
- ADC
- DAC
- DSP
- And more, but I really wanted that DSP and DAC
- I install STM32CubeMX on my Mac M1 (with some troubles at first, but it works).
- I select the board I just ordered.
- Let the software do its stuff and then the DAC configuration is in RED in the "pinout & configuration" panel because it conflict with GPIO PA5.
- GPIO PA5 have the user label "LD2 [Green LED]"
I'm flabbergasted. This is ridiculous, right ? why would I want a 1MS 12Bit DAC on a led ?
Despite my best effort browsing the documentation, as a beginner to the STM ecosystem, I understand that it's hardwired to PA5:
Table 9. STM32F410x8/B pin definitions, page 36/143 of the STM32F410x8 STM32F410xB datasheet.
Is the PA5 really hardwired to a (green) led on this board ?
Is there something I can do to use the DAC ?
Can the pinout be changed ?
Is there another M4 board in a < 100 euro price range with DAC & DSP ?
(i also ordered an Adafruit board at the same time with a microchip mcu in order to try their circuit python thing, but I would like to have a STM board too )
Thank you.