Skip to main content
Dion Hicks
Visitor II
June 19, 2017
Question

NUCLEO-F302R8 Evaluation Board Code using the SW4STM32 (AC6 Tools) IDE

  • June 19, 2017
  • 0 replies
  • 342 views
Posted on June 19, 2017 at 20:38

I am trying to get the base code for the NUCLEO-F302R8 evaluation board working using the SW4STM32 (AC6 Tools) IDE.  I've downloaded the X-NUCLEO-IHM07M1 pack from the website and after having to change the link to many files I was able to get it to build correctly.  The directory I am using for the project is:

..\STM32CubeExpansion_SPN7_V1.0.0\Projects\Multi\Examples\MotorControl\SW4STM32\STM32F302R8-Nucleo

However, I am not able to get the debugger to work.  I have other projects which use the same debugger with the directories for GDB and OpenOCD being the same in both projects.  When trying to debug I end up getting the following error message in a pop-up window: 

Error in final launch sequence

Failed to execute MI command:

load C:\\Users\\User\\Desktop\\en.X-CUBE-SPN7\\STM32CubeExpansion_SPN7_V1.0.0\\Projects\\Multi\\Examples\\MotorControl\\SW4STM32\\STM32F302R8-Nucleo\\Debug\\STM32F302R8-Nucleo.elf

Error message from debugger back end:

Load failed

Load failed

Does anyone have a solution to this issue?

    This topic has been closed for replies.