Skip to main content
Ran Kai
Associate
Aug 24, 2017 5:45 PM UTC
Question

Nucleo-f070rb bootloader

Posted on August 24, 2017 at 19:45

My board is connected with usb-ttl board and I can communicate with uart using HAL drivers.  I am trying to connect using STMFlashLoader Demo app from ST but I keep getting No response from the target,...

So far I have tried boot0 pin set to 1 and jump to system flash using code but it seems there is no connection, I see no response from the target on the scope either.  I cant find anything in the AN2606 and must be missing some critical piece of information.  any help would be great.

Thanks

    This topic has been closed for replies.