Nucleo-C092RC No ST-LINK detected
- 1 reply
- 0 views
Hi I have been at this for a couple of hours and I cannot figure out how to upload a program onto my Nucleo-C092RC that I bought from Digikey. I am using the STM32Cube IDE v2.20 on a Windows 11 PC, as well as the CubeProgrammer and CubeMX
I have followed the tutorial from this video to create a simple Blink LED example:
When I got to the stage where I go into debug mode and upload the code to my C092RC I get the error “No ST-LINK detected. Please connect ST-LINK and restart the debug session”. I have gone through the below help article as well as suggestions from the STM32 sidekick and have been unsuccessful so far. The only thing I haven't tried from the below help article is the Mass erase MCU
In device manager I see both “STMicroelectronics STLink Virtual COM Port” under Ports (COM & LPT) and I see “ST-Link Debug” under Universal Serial Bus devices. When I connect to the C092RC directly via USB from my PC I see the green power LED LD3, the solid red LD4, and LD1 and LD2 are alternating. I am fairly certain that I have the correct jumpers in place (I didnt move any of them since unboxing). From what I can tell I shouldn't need one of the programming dongles (ST-LINK/V2).
I have tried re-updating the ST-Link drivers as suggested by the STM32 sidekick but none of the solutions seemed to have worked. I CAN successfully connect to the board using the STM32CubeProgrammer. When I connect the LD4 flashes red/green and then is solid green for a few seconds.
Any help would be greatly appreciated!