Skip to main content
NJasa.1
Associate
Feb 6, 2021 9:58 AM UTC
Solved

Nucleo board for STM32F373

Hi,

Is nucleo board available for STM32F373 device? If not then any nucleo board can replace device with STM32F373?

Nandish

This topic has been closed for replies.
Uwe Bonnes
Uwe BonnesBest answer
Chief
Feb 6, 2021 4:36 PM UTC

Some L4 have a Sigma/Delta Interface too, see https://www.st.com/en/microcontrollers-microprocessors/stm32l4-series.html. Before you start with the F373 SDADC, have a look at the Gain error specifcation: -2.4 ..-2.7 ..-3.1%. Without a multiplexer to calibrate the gain you will be far off.

6 replies

Uwe Bonnes
Chief
Feb 6, 2021 12:32 PM UTC

There is no ST Demo board for the F373. I feel the SDADC of the F373 is not usefull, as the ADC gain is very variable. Consider e.g. some L4 with oversampling mode. It is a newer chips with many advantages as the peripherals are newer and more RAM

NJasa.1
NJasa.1Author
Associate
Feb 6, 2021 12:38 PM UTC

Thanks Uwe Bonnes,

In my application i have to measure three phase voltage and current measurements and i feel Sigma-Delta will give accurate measurement, that is why i select F373, again i will check L4, meantime can you please tell me that L4 can use for three phase voltage and current measurement?

Nandish

Tesla DeLorean
Guru
Feb 6, 2021 3:38 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Uwe BonnesBest answer
Chief
Feb 6, 2021 4:36 PM UTC

Some L4 have a Sigma/Delta Interface too, see https://www.st.com/en/microcontrollers-microprocessors/stm32l4-series.html. Before you start with the F373 SDADC, have a look at the Gain error specifcation: -2.4 ..-2.7 ..-3.1%. Without a multiplexer to calibrate the gain you will be far off.

NJasa.1
NJasa.1Author
Associate
Feb 8, 2021 8:01 AM UTC

Thanks Uwe Bonnes,

I have go through L4 devices and its seems to be applicable to my application. I will try on that. i am little bit greed, is any L4 device having Ethernet MAC10/100?

Nandish.

Piranha
Principal III
Feb 6, 2021 7:06 PM UTC

In addition the basic SAR 12-bit ADC on L4 has an up to 256x hardware oversampling with internal 20-bit summing and up to 16-bit data output.