Skip to main content
ronen yacobi
Associate II
Oct 10, 2017 8:34 PM UTC
Question

Nucelo STM32F429ZI with 8742A PHY

Posted on October 10, 2017 at 22:34

Hi,

I am using the latest ST32CubeMx Ver. 4.22.

Creating a new project with the wizard and selecting my target board Nucelo STM32F429ZI.

When selecting the middleware ETH connectivity I have DP8348 as only choice where the board is with PHY from Microchip 8742A. Since the board is not really new I thought this should be known already..

I can see that something with ETH init is to read over the DMA that the PHY has gone through reset which means sending other info then 0x0 I guess

/* Wait for software reset */

while (((heth->Instance)->DMABMR & ETH_DMABMR_SR) != (uint32_t)RESET)

didn't dig into it yet, thought I can ask here before what should be changed to get it working...

    This topic has been closed for replies.

    2 replies

    ronen yacobi
    Associate II
    Oct 11, 2017 1:16 PM UTC
    Posted on October 11, 2017 at 15:16

    1. SysTick_Handler call osSystickHandler, but none of them increments

    the tick counter. Don't why, I added this at the begining of the

    osSysTickHanlder

    osSystickHandler

    {

        HAL_IncTick();

     -----

    }

    2. TICK_INT_PRIORITY made the highest since I am calling for HAL_delays

    in different tasks.

    #define  TICK_INT_PRIORITY            ((uint32_t)0U)   /*!< tick

    interrupt priority */    

    3. Last... and most important are the corrected settings for the PHY8742A

    https://github.com/ronen-yacobi/LwIp_TcpUdp_EchoServer.git

     
    Vangelis Fortounas
    Associate II
    Oct 11, 2017 4:32 PM UTC
    Posted on October 11, 2017 at 18:32

    Hello!

    Try to use R.MII mode.

    0690X00000608XZQAY.png

    And for the systick , you must avoid to use Systick timer  for HAL when you use also a RTOS.

    Use another timer  to avoid theese problems.

    The generated code will include HAL_IncTick(); in Timers IRQ handler.

    0690X00000608ZiQAI.png

    Regards

    vf