Skip to main content
denisb-popov
Associate II
December 9, 2015
Question

NSS stays low after disabling SPI

  • December 9, 2015
  • 0 replies
  • 433 views
Posted on December 09, 2015 at 16:00

MCU: stm32f103rf

SPI: SPI1 without remap, MSTR = 1

SPI1 NSS pin PA4 configured as AF push-pull

PA4 remains low independent of SPI state (SPE, SSOE). When PA4 configured as GPIO it is working fine.

When running the same code with remaped SPI1 (also remap to SWD), NSS pin(PA15) goes high after it's configuration and enabling SPI1 clock (in any order).

Then it goes low after {SSOE = 1;  SPE =1}. Then it goes high after SPE = 0.

    This topic has been closed for replies.