Senior III
December 30, 2021
Question
Now impossible to design with STM32 due to no stock and/or crazy prices - is it going to change?
- December 30, 2021
- 8 replies
- 3426 views
I' ve just visited the JLC website and this is the current stock of STM32. My open source design for a STM32H743 based computer is now dead as there aren't any. Matek, the developer of flight controllers for drones has stopped production because of a combination of cost and lack of availability of processors.
Another design I did for one of the 64-pin H7 processors is also dead as AFAIK they have never seen silicon since their announcement.
Even prices for things like F411 / F407 are going through the roof.
Is this ever going to change or should I just give up on ST?