Skip to main content
MKnap.1
Associate
Jan 5, 2021 11:18 AM UTC
Solved

Not sure to whom to address my question: Question about Virtual Com-Port-Driver 1.3.1.0 installed on WIN10. The manager states "STMicroelectronics Virtual COM Port (COM 6)". But my attached ext. divice, which I want to access only accepts port 4!?

How can I change the driver to port 4 or how can I install the driver additionally for port 4?

*Edited by moderation: please don't mention your email address publicly on this forum*

    This topic has been closed for replies.
    MKnap.1
    MKnap.1Best answer
    Associate
    Jan 6, 2021 11:32 AM UTC

    Thanks for this additonal hint. So in future whenever I need to connect to my external device I first will check if the port managed by windows is still the same. In case it changed I also have to modify my configuration file.

    4 replies

    Peter BENSCH
    ST Technical Moderator
    Jan 5, 2021 12:40 PM UTC

    The port number is exclusively managed by Windows and cannot (simply) be changed to a specific number. A particular program will usually find the port number(s) automatically or display a list from which it can be selected. Additionally, you can open the Device Manager (as you have already done) and check the VCOM port number of the current device.

    Perhaps you could explain what exactly you mean by "only accepts port 4" as the device should only write to or read from a UART connected to the USB MCU?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    MKnap.1
    MKnap.1Author
    Associate
    Jan 5, 2021 5:39 PM UTC
    Dear Mr. Bensch, thank you so much for your time and explanation. Meanwhile I found out that my program which connects via USB to the external device has a configuration file in which the port can be modified by a text-editor. Like this I modified to the port shown like in the device manager. So my problem is solved. Thanks again and have a nice day. Matthias Knapp Am Di., 5. Jan. 2021 um 13:40 Uhr schrieb ST Community :
    Peter BENSCH
    ST Technical Moderator
    Jan 6, 2021 7:35 AM UTC

    You are welcome!

    Please note that the port number is assigned dynamically and can even change on a given Windows machine. So it may not be a good idea to set this up in a configuration file.

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    MKnap.1
    MKnap.1AuthorBest answer
    Associate
    Jan 6, 2021 11:32 AM UTC

    Thanks for this additonal hint. So in future whenever I need to connect to my external device I first will check if the port managed by windows is still the same. In case it changed I also have to modify my configuration file.