Skip to main content
Ukazu
Associate III
March 6, 2024
Solved

Not a genuine ST Device!

Hi

I would like to debug STM32F303RDT6 using a combination of Keil and ULINK2.
When I start debugging on the target microcontroller (STM32F303RDT6), **Not a genuine ST Device! Abort connection** is output as shown below.

We investigated the cause.
I found the following files.
**C:\Keil_v5\ARM\PACK\.Web\Keil.STM32F3xx_DFP.pdsc**

It seems that this process is failing.

```xml
        <!-- User-Defined Sequences -->
        <sequence name="CheckID">
          <block>
            __var pidr1 = 0;
            __var pidr2 = 0;
            __var jep106id = 0;
            __var ROMTableBase = 0;

            __ap = 0;      // AHB-AP

            ROMTableBase = ReadAP(0xF8) &amp; ~0x3;

            pidr1 = Read32(ROMTableBase + 0x0FE4);
            pidr2 = Read32(ROMTableBase + 0x0FE8);
            jep106id = ((pidr2 &amp; 0x7) &lt;&lt; 4 ) | ((pidr1 &gt;&gt; 4) &amp; 0xF);
          </block>

          <control if="jep106id != 0x20">
            <block>
              Query(0, "Not a genuine ST Device! Abort connection", 1);
              Message(2, "Not a genuine ST Device! Abort connection.");
            </block>
          </control>
        </sequence>
```

 Below is the keil log.

```
14:13:16:247 (05/03/2024) - START SEQUENCE "DebugDeviceUnlock", "calling sequence" - ID 19
14:13:16:251 (05/03/2024) - READ  AP  Access, AP 0, Addr 0x000000F8, Val 0xE00FF003, "SWD Read AP - Success" - ID 3
14:13:16:257 (05/03/2024) - READ  MEM BLOCK Access, AP 0, Start Addr 0xE00FFFE4, End Addr 0xE00FFFE7, "SWD Read Memory Block (32-bit accesses) - Success" - ID 4
  Item #0, AP 0, Addr 0xE00FFFE4, Value 0x00000040
14:13:16:261 (05/03/2024) - READ  MEM BLOCK Access, AP 0, Start Addr 0xE00FFFE8, End Addr 0xE00FFFEB, "SWD Read Memory Block (32-bit accesses) - Success" - ID 5
  Item #0, AP 0, Addr 0xE00FFFE8, Value 0x0000005C
14:13:57:001 (05/03/2024) - END SEQUENCE "InitTarget", "failed" - ID 20
```

pidr1 is 0x00000040
pidr2 is 0x0000005C

An error occurs because the following processing does not result in 0x20.

```
jep106id = ((pidr2 &amp; 0x7) &lt;&lt; 4 ) | ((pidr1 &gt;&gt; 4) &amp; 0xF);
```

What is the cause of this?
This topic has been closed for replies.
STOne-32
STOne-32Best answer
ST Technical Moderator
March 8, 2024

Dear @Ukazu ,

We confirm the part is genuine and we shipped it to our distributor DigiKey . So it might be a connection issue  due to hardware power supply or anything else you need to investigate. If you can Try with our STM32CubeProgrammer and have the log file please .

Cheers,

STOne-32

10 replies

Ukazu
UkazuAuthor
Associate III
March 6, 2024

Help Me!!

Tesla DeLorean
Guru
March 6, 2024

>>What is the cause of this?

Probably counterfeit parts..

Perhaps a large, close, sharp, well focused picture of the top markings of the IC ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ukazu
UkazuAuthor
Associate III
March 7, 2024

Hi

 

@Tesla DeLorean 

Thank you very much.
I'm interested in your answer.

Does that mean I bought a fake?
This is a problem.

 

I would also like to hear opinions from ST microelectronics engineers! !

Tesla DeLorean
Guru
March 7, 2024

Ok, but they are not psychic either, so without some markings, or trace codes from the packaging, or knowing how these part(s) were sourced it's going to be hard to know.

You could try also accessing with an ST-LINK and STM32 Cube Programmer

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
STOne-32
ST Technical Moderator
March 7, 2024

Dear @Ukazu ,

 « When I start debugging on the target microcontroller (STM32F303RDT6), **Not a genuine ST Device! Abort connection** »

is that correct the flash programming ( Erase and write , has been done successfully first on this part) and then when starting to debug : you got this message ?  
if possible indeed to have the product Top marking on this LQFP64 package and if possible the UID - unique ID signature so we can  check it from our factory side .

Ciao

STOne-32

Ukazu
UkazuAuthor
Associate III
March 7, 2024

@STOne-32 

No, it is not possible to erase or write to flash. Therefore, debugging cannot be started.

I tried two combinations: Keil+ULINK2 and Keil+STLINK, but they were unsuccessful.

I purchased this microcontroller from an online shop. A world-famous online shop for device parts.

 

I don't have a target microcontroller at the moment, so I don't know the TOP marking.

We will contact you as soon as we know.

 

Thank you

STOne-32
ST Technical Moderator
March 7, 2024

Dear @Ukazu ,

if you can have a picture of the device marking as below :

IMG_6797.jpeg

Thank you 

STOne-32
STOne-32Best answer
ST Technical Moderator
March 8, 2024

Dear @Ukazu ,

We confirm the part is genuine and we shipped it to our distributor DigiKey . So it might be a connection issue  due to hardware power supply or anything else you need to investigate. If you can Try with our STM32CubeProgrammer and have the log file please .

Cheers,

STOne-32

Ukazu
UkazuAuthor
Associate III
March 10, 2024

@STOne-32 

 

Thank you for your investigation.
I was relieved that the results were genuine.

I will check again to make sure there are no problems with the circuit or wiring, etc. as advised.