Skip to main content
rgalbany2
Associate
March 23, 2011
Question

NO ST-Link Detected with MDK-ARM

  • March 23, 2011
  • 12 replies
  • 3600 views
Posted on March 23, 2011 at 08:14

Hello,

I'm totally novice and need your help.

I have installed the lastest version of the MDK-ARM from keil.

The result of the compilation is good, but when try to download the programm to the uC, the Software launch one message: ''

NO ST-Link Detected

''.

When I connect the DISCOVERY board to my USB, the led Blinks correctly, and 

and

I

could

update

the

firmware

of

the

system without

problems

.

Where is my problem?

Thanks!
    This topic has been closed for replies.

    12 replies

    rgalbany2
    rgalbany2Author
    Associate
    April 5, 2011
    Posted on April 05, 2011 at 08:25

    Hi!

     

     

    tested!! the Discovery board works fine with WinXP in english, but don't works if the language is in Spanish !!!!! Using Vista & Spanish language also don't woks!!

     

     

    The past week I have sent one email to ST, but not have receiver any reply yet. Please correct this BUG Sirs of ST !!!

     

     

    Regards,

     

     

    Raul.
    evgentusbachinintus
    Visitor II
    July 27, 2012
    Posted on July 27, 2012 at 02:57

    I find a short video about this problem which advices some ways to solving this problem. I was approached last piece of advice

     Here is the Youtube Link  

    http://www.youtube.com/watch?v=2mNc-v-OWSY&feature=plcp