Skip to main content
Associate
Aug 13, 2025 10:41 AM UTC
Solved

No ST-LINK detected! Please connect ST-LINK and restart the debug session.

hello,

i am working on project with a stm32wle5jc and am fairly new to stm tools. all was working well but after a little break on another project it will no longer flash the board with the stm ide (1.19.0) and says "No ST-LINK detected! Please connect ST-LINK and restart the debug session.". i have an st-link/v2 connected and the ide can actually see the st-link under "help" "st-link upgrade" (i am on a macbookpro m1, which also sees the st-link under "system report", "usb")

i can flash the code i want to flash from the ide (~/workspace/<projectname>/Debug/<projectname>.elf) with the stmcubeprogrammer without any problem

i have restarted the ide, restarted the mac, switched cables, switched projects, switch boards, tried a st board nucleo board with embedded st-link (or whatever it is)... but always get the same error message

what is going on?

any help greatly appreciated!

thanks, frank

This topic has been closed for replies.
frbBest answer
Associate
Aug 13, 2025 11:16 AM UTC

finally! problem fixed.

found a post  on stackoverflow which solved the problem by reinstalling st-link server

fixed the problem!

1 reply

frbAuthorBest answer
Associate
Aug 13, 2025 11:16 AM UTC

finally! problem fixed.

found a post  on stackoverflow which solved the problem by reinstalling st-link server

fixed the problem!