No scroll bars in STM32MX 5 GPIO config?
First let me say I love CUBE. I make it a point now to use ST parts when ever possible just because CUBE makes things so easy. However, the last two projects I worked on had CUBE (OK, the code generator firmware under CUBE) bugs that took a while to find. One with the RTC on an l476 part and clock generation on a l107 part.
That said, am pretty disappointed in 5.0. I don't know why vendors feel they need to take a wonderful product, and just change it without adding any new functionality to speak of.
I can deal with most 5.0 issues and I still love CUBE but I have found that "System View" / "GPIO" does not seem to have scroll bars. When a part with a very high pin count is used some of the pins are not visible and there is no convenient way to get to them. Worse, when you click on a pin the config window for that pin pops up blocking even more pins.
I only see two work arounds
1) Get a very high resolution monitor with small font
2) Click on a pin I can see, then use the arrows to move up and down the list. This at least lets me see / change the pin's data in the config window even though I can't see it in the pin list. Not being able to see the complete list of pins and how they are configured makes things awkward.
Am I just missing something? If not, when will scroll bars be added?