Skip to main content
Nipuni Perera
Associate II
Feb 7, 2018 5:10 AM UTC
Solved

no response from usart - stm32f3 discovery

Posted on February 07, 2018 at 06:10

I have been trying to get the USART to work on the stm32f3 discovery for a while without any success. Currently, the TX pin (PA2) is at a constant 3.3V, the RX pin (PA3) is at a constant 0V. I am using an FTDI Basic breakout board to read the USART, and I am using the keil uvision 5 IDE.

The code is given below:

/* Includes ------------------------------------------------------------------*/

&sharpinclude <stm32f30x.h>

&sharpinclude <stm32f30x_rcc.h>

&sharpinclude <stm32f30x_rcc.c>

&sharpinclude <stm32f30x_gpio.h>

&sharpinclude <stm32f30x_gpio.c>

&sharpinclude <stm32f30x_misc.h>

&sharpinclude <stm32f30x_misc.c>

&sharpinclude <stm32f30x_tim.h>

&sharpinclude <stm32f30x_tim.c>

&sharpinclude <stm32f30x_usart.h>

&sharpinclude <stm32f30x_usart.c>

//&sharpinclude <arm_math.h>

/* Private typedef -----------------------------------------------------------*/

/* Private define ------------------------------------------------------------*/

/* Private macro -------------------------------------------------------------*/

/* Private variables ---------------------------------------------------------*/

volatile int ms;

/* Private function prototypes -----------------------------------------------*/

/* Private functions ---------------------------------------------------------*/

void SysTick_Handler(void)

{

  ms++;

}

/**

  * @brief  Main program.

  * @param  None

  * @retval None

  */

int main(void)

{

  GPIO_InitTypeDef GPIO_InitStruct;

    USART_InitTypeDef USART_InitStruct;

    NVIC_InitTypeDef NVIC_InitStruct;

    

    /*GPIO configuration for indicator LED*/

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE,ENABLE);

    

    GPIO_InitStruct.GPIO_Pin = GPIO_Pin_8|GPIO_Pin_9|GPIO_Pin_10|GPIO_Pin_11|GPIO_Pin_12;

    GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;

    GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;

    

    GPIO_Init(GPIOE,&GPIO_InitStruct);

    

    //Turn LED on

    GPIO_SetBits(GPIOE,GPIO_Pin_8|GPIO_Pin_12);

    

    /*GPIO configuration for USART. PA2 = USART2_TX, PA3 = USART2_RX*/

    //Enable clock for GPIOA

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA,ENABLE);

    

    GPIO_InitStruct.GPIO_Pin = GPIO_Pin_2|GPIO_Pin_3;

    GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;

    GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;

    

    GPIO_Init(GPIOA,&GPIO_InitStruct);

    

    //AF configuration

    GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_7);

    GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_7);

    

    /*USART configuration*/

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE);

    USART_Cmd(USART2, ENABLE);

    

    USART_InitStruct.USART_BaudRate = 9600;

    USART_InitStruct.USART_WordLength = USART_WordLength_8b;

    USART_InitStruct.USART_StopBits = USART_StopBits_1;

    USART_InitStruct.USART_Parity = USART_Parity_No;

    USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    USART_InitStruct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  USART_Init(USART2, &USART_InitStruct);

    

    //Enable RXNE interrupt

    USART_ITConfig(USART2,USART_IT_RXNE,ENABLE);

    GPIO_SetBits(GPIOE,GPIO_Pin_9);

    //Enable USART global interrupt

    //NVIC_EnableIRQ(USART2_IRQn);

    NVIC_InitStruct.NVIC_IRQChannel = USART2_IRQn;

    NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0;

    NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStruct);

    GPIO_SetBits(GPIOE,GPIO_Pin_10);

    

    if (SysTick_Config(SystemCoreClock / 1000))

  {

    /* Capture error */

    while (1);

  }

    GPIO_SetBits(GPIOE,GPIO_Pin_11);

    

  while (1)

  {

        if (ms>99){

            USART_SendData(USART2,'S');

            while(USART_GetFlagStatus(USART2,USART_FLAG_TXE)==RESET){};

            if (GPIO_ReadOutputDataBit(GPIOE,GPIO_Pin_12)){

                    GPIO_ResetBits(GPIOE,GPIO_Pin_12);

            }

            else{

                    GPIO_SetBits(GPIOE,GPIO_Pin_12);

            }

            ms=0;

        }

  }

}

void USART2_IRQHandler(void){

    //RXNE handler

    if(USART_GetITStatus(USART2,USART_IT_RXNE) != RESET){

        //If recieved 't', toggle LED, transmit 'T'

        if((char)USART_ReceiveData(USART2) == 't'){

            //Toggle LED

            if (GPIO_ReadOutputDataBit(GPIOE,GPIO_Pin_8)){

                GPIO_ResetBits(GPIOE,GPIO_Pin_8);

            }

            else{

                GPIO_SetBits(GPIOE,GPIO_Pin_8);

            }

            

            USART_ClearITPendingBit(USART2,USART_IT_RXNE);

            //USART_SendData(USART1,'T');

            //while(USART_GetFlagStatus(USART2,USART_FLAG_TXE)==RESET){}

        }

    }

}

#stm32f3-discovery #usart
This topic has been closed for replies.
Tilen MAJERLE
Tilen MAJERLEBest answer
ST Employee
Feb 7, 2018 3:17 PM UTC
Posted on February 07, 2018 at 16:17

st118581

‌,

you should not enable UART before you configure it. First do the configuration, afterUART_Init function callUART_Cmd and enable it.

Best regards,

Tilen

3 replies

Tilen MAJERLE
Tilen MAJERLEBest answer
ST Employee
Feb 7, 2018 3:17 PM UTC
Posted on February 07, 2018 at 16:17

st118581

‌,

you should not enable UART before you configure it. First do the configuration, afterUART_Init function callUART_Cmd and enable it.

Best regards,

Tilen

Tesla DeLorean
Guru
Feb 8, 2018 12:41 AM UTC
Posted on February 08, 2018 at 00:41

Would also recommend checking TXE *before* writing to the data register, you're trying to ensure the register is empty, not wait for it to transit or move to the shift register.

...

    USART_Init(USART2, &

USART_InitStruct)

;

    USART_Cmd(USART2, ENABLE);

...

            while(USART_GetFlagStatus(USART2,USART_FLAG_TXE)==RESET){};

            USART_SendData(USART2,'S');

...

https://community.st.com/0D50X00009XkgXFSAZ

 
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
T J
Senior III
Feb 7, 2018 11:21 PM UTC
Posted on February 08, 2018 at 00:21

The Rx pin should not be Low....

before the Uart will function this pin should be high...