Skip to main content
yfbaidyj
Associate
November 14, 2008
Question

no output of USART with STM32-H103 board

  • November 14, 2008
  • 1 reply
  • 629 views
Posted on November 14, 2008 at 07:15

no output of USART with STM32-H103 board

    This topic has been closed for replies.

    1 reply

    yfbaidyj
    yfbaidyjAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:52

    Hallo everybody,

    I am new with the Cortex M3 and have some problems using the UART. I can´t see any output on Windows Terminal. I use CrossStudio for ARM with Olimex ARM-USB-OCD and this is the source codes :

    void RCC_Configuration(void)

    {

    RCC_DeInit();

    // 2. Enable ext. high frequency OSC

    RCC_HSEConfig(RCC_HSE_ON);

    // wait until the HSE is ready

    while(RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET);

    // 3. Init PLL

    RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_9); // 72MHz

    RCC_PLLCmd(ENABLE);

    // wait until the PLL is ready

    while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET);

    // 4. Set system clock divders

    /* RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5); */

    RCC_HCLKConfig(RCC_SYSCLK_Div1); // AHB Clock = 72 MHz

    RCC_PCLK2Config(RCC_HCLK_Div1);

    RCC_ADCCLKConfig(RCC_PCLK2_Div8); // ADC Clock = 8 MHz

    RCC_PCLK1Config(RCC_HCLK_Div2);

    // Flash 1 wait state

    *(vu32 *)0x40022000 = 0x12;

    // 5. Clock system from PLL

    RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

    while(RCC_GetSYSCLKSource() != 0x08)

    {

    }

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO | RCC_APB2Periph_ADC1 |RCC_APB2Periph_AFIO | RCC_APB2Periph_USART1, ENABLE);

    }

    int main (void)

    {

    #ifdef DEBUG

    debug();

    #endif

    /* System clocks configuration ---------------------------------------------*/

    RCC_Configuration();

    // Configure PA.9 (USARTT1_TX) as output Open Drain Output Alternate-Function

    GPIO_ResetBits(GPIOA,GPIO_Pin_9);

    GPIO_InitStruct.GPIO_Pin = GPIO_Pin_9;

    GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_OD;

    GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_Init(GPIOA, &GPIO_InitStruct);

    USART_Configuration();

    USART_Cmd(USART1, ENABLE);

    while(1)

    {

    USART_SendData(USART1, 0xaa);

    while(!USART_GetFlagStatus(USART1, USART_FLAG_TXE))

    {

    }

    while(!USART_GetFlagStatus(USART1, USART_FLAG_TC))

    {

    }

    }

    }

    /*******************************************************************************/

    void USART_Configuration(void)

    {

    USART_InitTypeDef USART_InitStruct;

    /* Configure -------------------------*/

    USART_InitStruct.USART_BaudRate = 9600; /* 9600 Baud */

    USART_InitStruct.USART_WordLength = USART_WordLength_8b;

    USART_InitStruct.USART_StopBits = USART_StopBits_1;

    USART_InitStruct.USART_Parity = USART_Parity_No ;

    USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    USART_InitStruct.USART_Mode = USART_Mode_Tx;

    /* USART_InitStruct.USART_Clock = USART_Clock_Enable;

    USART_InitStruct.USART_CPOL = USART_CPOL_Low;

    USART_InitStruct.USART_CPHA = USART_CPHA_1Edge;

    USART_InitStruct.USART_LastBit = USART_LastBit_Disable; */

    USART_Init(USART1, &USART_InitStruct);

    }

    I have tested the output of UART Tx Pin with oscilloscope but there is output signal. Before i have already test program loading by the simple ''blinky'' program and it´s ok.

    I really have no idea. Could someone help me ? thank u