Question
No output from DAC @STM32F103VExx
Posted on April 10, 2012 at 17:50
Hi,
I am a university undergrad and I am designing a Digital storage oscilloscope. I need the micro controller's DAC output for DC voltage. I have seen the sample code and I know how to setup the timer, link the DMA to DAC. The code seems to be working fine on STM32VLdiscovery board, but when I run it on my STM32F103VET6 processor there is no output from DAC i.e. 0V. I would like to clarify:- I have made the board myself but I have made sure that all the connections are as per the datasheet.- I have given Vref+ as 3.3V , Vref- as GND as well. All the decaps are in place too.- All other peripheral are working fine, it is just the DAC which does not seem to be working.One problem could be with the DAC 12-bit right align config adddress i.e. &sharpdefine DAC_DHR12RD_Address 0x40007420.I reckon this should be different for STM32f103VExx than STM32f100RBxx. The code is exactly the same as ''DualModeDMA_SineWave''. Thankyou #dac-dma-tim2