Skip to main content
MWILL.17
Associate
February 27, 2019
Question

No matter what i do the virtual com port will not show up using STM Defuse Demonstrator.

  • February 27, 2019
  • 4 replies
  • 1790 views

Im trying to set up a KISS FC and i can not get it to connect so i followed some tutrials and used the software but nothing is showing up so i cant complete any of the tutorials.

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    February 27, 2019

    DfuSe Demo doesn't use a COM port, it is looking for an "STM32 Device in DFU Mode". For devices that support that, you need to restart the STM32 with the BOOT0 pulled HIGH, while being plugged into the USB connector.

    The STM32 Cube Programmer tools can use the System Loader's USART or USB modes of operation.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    MWILL.17
    MWILL.17Author
    Associate
    February 27, 2019

    im not even going to try and pretend to have any idea how to do that. I am just having an extremely hard time with this tutorial on how to get my device connected and nothing i am doing is causing the stm32 bootloader or anything to show up in my device manager so that i can connect.

    MWILL.17
    MWILL.17Author
    Associate
    February 27, 2019

    I understand that bootloader is not the correct driver im lookiong for either but STM Device in DFU Mode never shows up for me.