Skip to main content
John Hite
Associate III
Mar 20, 2017 7:10 PM UTC
Solved

No interrupt on tmr overflow

Posted on March 20, 2017 at 20:10

STM32F437

I am using TIM4 for input capture and an interrupt occurs when external events occur. However I stopped the external event and no interrupt occurs on overflow although the UIF bit is set in SR. Code snippet below and TIM4 is listed below that.

Thank you,

JH

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

void RpmTask(void *p_arg)

{

  TIM_TypeDef *tim4 = TIM4;

  RCC_TypeDef *rcc = RCC;

  OS_ERR err;

  uint16_t rpm4 = 0;

  NVIC_InitTypeDef NVIC_InitStruct;

  /*Interrupt packet initialization*/

  NVIC_InitStruct.NVIC_IRQChannel = TIM4_IRQn;

  NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 1;

  NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStruct);

 

  //RPM timer setups

  // APB1PeriphClock - 42 MHz

  // APB2PeriphClock - 84 MHz

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3 | RCC_APB1Periph_TIM4, ENABLE);

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 | RCC_APB2Periph_TIM9, ENABLE);

  TIM_TimeBaseInitTypeDef tim4_base;

  tim4_base.TIM_Period = 0xFFFF;

  tim4_base.TIM_Prescaler = 0; //42000 -1;

  tim4_base.TIM_ClockDivision = TIM_CKD_DIV1;  //digital filter clk div, don't care, filtering is off

  tim4_base.TIM_CounterMode = TIM_CounterMode_Up;

  tim4_base.TIM_RepetitionCounter = 0; //t1&t8 pwm, don't care

  TIM_TimeBaseInit(TIM4, &tim4_base);

  TIM_ICInitTypeDef tim4_icInit;

  tim4_icInit.TIM_Channel = TIM_Channel_1;

  tim4_icInit.TIM_ICPolarity = TIM_ICPolarity_Rising; //r, f, both

  tim4_icInit.TIM_ICSelection = TIM_ICSelection_DirectTI; //dir, ind, trc

  tim4_icInit.TIM_ICPrescaler = TIM_ICPSC_DIV1; //1-8

  tim4_icInit.TIM_ICFilter = 0x0;

  TIM_ICInit(TIM4, &tim4_icInit);

 

  TIM_UpdateDisableConfig(TIM4, 0);

    

  /* Enable the CC2 Interrupt Request */

  TIM_ITConfig(TIM4, TIM_IT_CC1, ENABLE);

  /* TIM enable counter */

  TIM_Cmd(TIM4, ENABLE);

  uint16_t cnt = 0;

  while(1)

  {

    cnt = TIM_GetCounter(TIM4);

    OSTimeDlyHMSM(0u, 0u, 0u, 1000u, OS_OPT_TIME_HMSM_NON_STRICT, &err);

  }

}

void timer4_isr(void)

{

  volatile int optimizerBlock = 0;

  TIM_TypeDef *tim44 = TIM4;

  uint16_t rpm4 = 0;

  uint32_t cnt;

  CPU_SR_ALLOC();

 

  CPU_INT_DIS();

  OSIntNestingCtr++;

  CPU_INT_EN();

 

  if (TIM_GetITStatus(TIM4, TIM_IT_Update) == SET)

  {

    ...

     TIM_ClearITPendingBit(TIM4, TIM_IT_Update);

  }

 

 

  if (TIM_GetITStatus(TIM4, TIM_IT_CC1) == SET)

  {

    ...

   TIM_ClearITPendingBit(TIM4, TIM_IT_CC1);

  }

 

  OSIntExit();

}

Expression    Value    Location    Type    

tim4    0x40000800    R5    TIM_TypeDef *    

CR1    0x0001        

RESERVED0    

CR2    0x0000        

RESERVED1    

SMCR    0x0000    

RESERVED2    

DIER    0x0002    

RESERVED3    

SR    0x001D        

RESERVED4    

EGR    0x0000        

RESERVED5    

CCMR1 0x0001    

RESERVED6    

CCMR2 0x0000    

RESERVED7    

CCER    0x0001    

RESERVED8    

CNT    51557        

PSC    0x0000        

RESERVED9    

ARR    0x0000FFF

RCR    0x0000        

RESERVED10    

CCR1    0x00000000        

CCR2    0x00000000        

CCR3    0x00000000        

CCR4    0x00000000        

BDTR    0x0000    

RESERVED11    0x0000    

DCR    0x0000    0x40000848

RESERVED12    0x0000            

DMAR    0x0001    0x4000084C    

RESERVED13    0x0000            

OR    0x0000    0x40000850        

RESERVED14    0x0000            
    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Mar 20, 2017 7:49 PM UTC
    Posted on March 20, 2017 at 20:49

    TIM_ITConfig(TIM4, TIM_IT_Update, ENABLE); // Enable the Update

    It gates the UIF bit to the TIMx_IRQ pin and the NVIC

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    2 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Mar 20, 2017 7:49 PM UTC
    Posted on March 20, 2017 at 20:49

    TIM_ITConfig(TIM4, TIM_IT_Update, ENABLE); // Enable the Update

    It gates the UIF bit to the TIMx_IRQ pin and the NVIC

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    John Hite
    John HiteAuthor
    Associate III
    Mar 20, 2017 9:30 PM UTC
    Posted on March 20, 2017 at 21:30

    Thanks Clive,

    I OR'ed that puppy in with TIM_IT_CC1 and now she's banging on all cylinders.

    JH