Skip to main content
Associate II
May 17, 2024
Question

No device found on target error while dumping customized code for second time in STM32H735uC

Hi,

     I have an application code(Call it as Code-1). I able to dump it into my custom STM32H735  board through ST-LINK V3 MINIE. But when i try to dump same code for second time, it showing below error,

" Target no device found"

Error in Initializing ST Link Device.

Reason: NO device found on target."

I have 2nd board, Field working code(Code-2). I Can able to dump this Code-2  into 2nd board multiple times. But when i tried to dump Code-1 into 2nd board, for first time i able to dump it. When i tried for 2nd time it showing same error as shown above.

I understand that the Code-1 modified SWD pin configurations(unintentionally), due to which second time ST Link is being not detected.

How to solve this problem?? Please suggest.

Thanks in advance,

Pavani

 

 

This topic has been closed for replies.