Skip to main content
gds23
Associate II
May 11, 2010
Question

No bits in RCC_CSR at power-on

Posted on May 11, 2010 at 19:43

No bits in RCC_CSR at power-on

    This topic has been closed for replies.

    2 replies

    gds23
    gds23Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:50

    If I poll the RCC_CSR reg at least 3 times I then see the ''reset reason'' bits appear after an unclean reset. Contracted ST app engineers. So far they have not confirmed or denied but, for now, this wfm:

    main()

    {

    for (int i=0; i<10; i++)

        if (RCC->CSR & 0xFF000000)

             break;

    :

    :

    Ric Ricardo
    Visitor II
    June 5, 2018
    Posted on June 05, 2018 at 13:39

    I have a similar problem with the RCC->CSR register, especially with the IWDG Reset Status bit.

    Time Content of RCC->CSR

    After power on and enabling IWDG 0x14000003

    Then maybe after a second or less 0x34000003

    If the status bits receive a clear right upon reading them for the first time with

    RCC->CSR |= RCC_CSR_MASK_RMVF;�?

    then the content of the RCC->CSR is 0x20000

    Is the information of the reset cause of IWDG lazy loaded into the CSR register?

    Have I missed a note somewhere that says something about the timing of this status bit?