Skip to main content
gaurav2
Associate II
June 7, 2016
Question

Newbie Q: Getting just GPIO to work with STM32CubeF0

Posted on June 07, 2016 at 06:00

I am just getting started on STM32 micro-code development for a custom board built around the STM32F072. I downloaded the CubeF0 and was able to build a few sample projects.

I now want to extract just the GPIO parts (stm32f0xx_hal_gpio.c) and use that with my main.c but it appears that I need to include and link many other HAL parts as well. What is the bare minimum and how do I start turning off un-needed pieces?

For example, I think GPIO needs RCC to set peripheral clock. Which is fine. But then ''hal_rcc.c'' requires that I need ''hal_rcc_ex.h'' (extended) also otherwise compile error. Then I need to include ''hal_gpio_ex.h'' as well. It doesn't seem to stop. More and more header and .C files are required.

Any tips appreciated. Thanks a bunch.
    This topic has been closed for replies.

    3 replies

    Nesrine M_O
    Associate
    June 7, 2016
    Posted on June 07, 2016 at 11:07

    Hi gaurav_stm,

    1.You can start from GPIO examples under the STM32F0 cube firmware package, you find the needed include parts for your project

    STM32Cube_FW_F0_V1.5.0\Projects\STM32F072B-Discovery\Examples\GPIO

    2.Also you can generate your own initialization C code (pins, clock tree, peripherals, middleware) using STM32CubeMX tool 

    3.For more details about CUBEMX please refer to the UM1718 User manual

    -Syrine-

    Tesla DeLorean
    Guru
    June 7, 2016
    Posted on June 07, 2016 at 17:09

    When you buy into this thick hardware abstraction layer model that's what's going to happen. Best to let the compiler/linker do dead code elimination on the pieces it needs.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    gaurav2
    gaurav2Author
    Associate II
    June 8, 2016
    Posted on June 08, 2016 at 19:10

    Folks, I made some progress with CubeF0 and USB CDC class to get printf working. However, no characters appear on the hyper-term. The code roughly looks like:

    USBD_HandleTypeDef USBD_Device;

    extern UART_HandleTypeDef UartHandle;

    void main(void)

    {

       uint8_t ch = 'a';

        HAL_Init();

        SystemClock_Config();

      

        /* Init Device Library */

        USBD_Init(&USBD_Device, &VCP_Desc, 0);

      

        /* Add Supported Class */

        USBD_RegisterClass(&USBD_Device, &USBD_CDC);

      

        /* Add CDC Interface Class */

        USBD_CDC_RegisterInterface(&USBD_Device, &USBD_CDC_fops);

      

        /* Start Device Process */

        USBD_Start(&USBD_Device);

        

        while (1) {

            status = HAL_UART_Transmit(&UartHandle, (uint8_t *)&ch, 1, 10);

        }

    }

    However, nothing comes out on the Hyper-terminal connected on Windows. The HAL_Transmit_UART is going through but I fear that somehow the UART transmit data struct is not connected to the USB CDC class buffer and/or some DMA issue. 

    I don't want to use DMA but not sure how to just be in polling mode and if the UART (huart->Instance->TDR) in stmf0xx_hal_uart.c is really giving the character to the CDC.

    I think that USB CDC class transmits a packet in the USBD_CDC_TransmitPacket() function where it calls

          USBD_LL_Transmit(pdev, CDC_IN_EP, hcdc->TxBuffer, hcdc->TxLength);

    Do I instead need to use HAL_UART_Transmit_IT() to transmit in interrupt mode for USB to recognize that data is pending? Otherwise I don't see how the HAL_UART_Transmit() connects to USB CDC. The _IT() version seems to connect via the UserTxBuffer[].

    Any pointers in making progress will help me. Thanks.