Skip to main content
jj_it
Associate II
August 4, 2008
Question

New, SMALLER Xtals for STM32...

  • August 4, 2008
  • 3 replies
  • 699 views
Posted on August 04, 2008 at 06:48

New, SMALLER Xtals for STM32...

    This topic has been closed for replies.

    3 replies

    jj_it
    jj_itAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:40

    Many have sought physically smaller 8MHz Crystals. I report/identify two devices below: a) 6x3mm and b) 5x3.2mm. Both are fundamental, smt.

    Both currently stock @ Digi-Key:

    a) 535-9628-1

    b) 644-1132-1

    Regards,

    gdp123a
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:40

    To save even more space, I've been considering using Murata Ceramic resonators (Model CSTCE_G...). It's 3.2mm by 1.3mm and has built-in load capacitors. The only downside I can see is that they are not as accurate as a crystal, but that's not a problem in my application.

    Has anyone tried these with the STM32?

    thanks,

    Greg

    stevemelnikoff9
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:40

    Hi Greg.

    Yes, we have a prototype board which uses a CSTCE8M00G52A, with a 220R series resistor. So far, it appears to work fine - though we haven't done temperature or EMC tests yet.

    Steve.