Skip to main content
16-32micros
Associate III
May 18, 2009 2:58 PM UTC
Question

New Library Compatible with CMSIS - Comments

Posted on May 18, 2009 at 16:58

New Library Compatible with CMSIS - Comments

    This topic has been closed for replies.

    36 replies

    jilisegiar
    Associate III
    May 17, 2011 11:06 AM UTC
    Posted on May 17, 2011 at 13:06

    Just copy the example content to project/template folder then follow the steps described in the readme file (section: How to use it ?)provided with the example.

    FYI:

    There is 2 configs in the template project:

    - STM3210B-EVAL: to configure the project for STM32 Medium-density devices

    - STM3210E-EVAL: to configure the project for STM32 High-density devices

    akramaiah
    Visitor II
    May 17, 2011 11:06 AM UTC
    Posted on May 17, 2011 at 13:06

    Quote:

    Just to follow up has anyone successfully done the port in Crossworks? I have got most of the library compiling but not STM32F10x_pwr, as I get ''error: selected processor does not support wfi''

    and ''error: selected processor does not support wfe''

    I also get a host of linker errors related to memory allocations/locations.

    Any help and support would be welcome.

    Hi,

    I am trying to port the FWLib from ST, to the new CMSIS compatible library in rowelys crossworks. Do you have any starting point, where I can start with. Any help would be greatfull.

    Regards,

    akr

    peterharrison9
    Associate II
    May 17, 2011 11:06 AM UTC
    Posted on May 17, 2011 at 13:06

    Do any of you have an example project using the CMSIS library with GNU (CodeSourcery perhaps) toolchain and a suitable Makefile? I am having quite a lot of trouble getting this working. Stuff builds in Ride7 but I can't write a successful project without it. Since I work on an iMac, this is a bit of a problem :)

    Also, it it possible to compile the CMSIS stuff into a linkable library? It seems to be too interdependent on the project sources for that.

    Pete

    tiago2
    Visitor II
    May 17, 2011 11:06 AM UTC
    Posted on May 17, 2011 at 13:06

    Does anyone have the link to download this lib, I cant find it anywhere.

    akramaiah
    Visitor II
    May 17, 2011 11:06 AM UTC
    Posted on May 17, 2011 at 13:06

    Hi Peter,

    Thanks for the post. I need to port to rowelys (uses gcc compiler), let me see if I could abel to get your makefile settings and linker settings ported to rowelys.

    Regards,

    akr

    peterharrison9
    Associate II
    May 17, 2011 11:06 AM UTC
    Posted on May 17, 2011 at 13:06

    I think I may have it now:

    http://www.micromouseonline.com/blog/2009/05/18/stm32-on-the-mac-the-st-peripheral-driver-library/

    Well, mostly anyway..