Skip to main content
Associate II
Nov 22, 2023 7:47 PM UTC
Solved

NETXDUO not working with enabled TrustZone

Hi everyone,

i'm currently facing some issues while using NetXDuo (in the NonSecure World) with TrustZone.

My current goal: Use Network stuff, i.e. be able to ping the board from my PC with NetXDuo running in the NonSecure World with activated TrustZone.

 

With an empty project, i do the following steps and assign the ETH to the NS world. Apart from that, the project is empty.
The steps are more or less taken from this example.

- ETH: `RMII` mode. Set RxBuffLen to `1536`
- ICACHE: (optional to disable the IDE warnings) `2-ways set associative cache` mode
- ThreadX: `Core`
- NetXDuo: NX Core, DHCP Client, Network Interfaces > Ethernet Interfacea and LAN8472. In the configuration:
 - Platform Settings > chose lan8742 for both options
 - Enable Interface Capability true
 - Memory Pool Size 30 * 1024
 - Generate Init Code true
 - IP Instance Thread Size 2 * 1024
 - Pool Size in number of Packets 10
 - Application Thread Stack Size 2 * 1024
- NVIC: Enable Ethernet Global Interrupt to Preemption Prio 7
- SYS: Timebase Source TIM6
- RCC: Enable High Speed Clock > DIGBYPASS Clock Source
- Pinout: Set Pin PG12 to `ETH_TXD1`. (By doing this, PG14 should be cleared)

 

If i run the project like this, the wati until an IP Address is ready semaphore get in app_netxduo.c does not return to TX_SUCCESS, i.e. the board is not pingable. 

 

What kinda confuses me is that if i do the steps above in an Project without TrustZone, everything works.

 

Anyone got an idea what might be my issue? I also tried to compare the .ioc files by hand in an editor and did not spot anything what might be a problem.

 

I'd appreciate any help or hints :)

Best,

funkii

This topic has been closed for replies.
funkiiBest answer
Associate II
Dec 7, 2023 10:06 AM UTC

Hi,

i finally managed to get it working! Thanks @STea for your help, I really appreciate it.

Steps to get it working:

Start Board Project with Trustzone enabled
Firmware Version v1.1.1

Clear pinout

ETH
 Mode RMII
 RxBuffLen 1536
 Set Pin PG12 to ETH_TXD1 (By doing this, PG14 should be cleared)

THREADX
 Core

NETXDUO
 NX Core
 Addons > DHCP > Client
 Network Interfaces > Ethernet interface, Ethernet Phy Interface > LAN8742
 Platform Settings > both lan8742

 Enable Interface Capability true
 memory pool size 30 * 1024
 Genreate Init Code true
 IP Instance Thread Size 2 * 1024
 Pool Size in number of Packets 10
 Application Thread Stack Size 2 * 1024

NVIC_NS
 Ethernet global Interupt > Enable, Preemption Priority 7

SYS
 Timebase Source TIM6 (Assign TIM6 to NS before)

RCC
 High speed Clock DIGBYPASS Clock source

GTZC_S
 Block-Based Memory Controller > MPCBB3 (SRAM3) > Memory Privilege Attributes Settings > Configure Memory > from full Not privileged
 (Setting the whole SRAM3 to not priviliged might not be the best idea from an security standpoint if you do other stuff on the board)

Manual change in Secure/Core/Inc/partition_stm32h573xx.h:
Set the 10th bit in NVIC_INIT_ITNS3_VAL (in my case line 554), so the line should look like this:
`#define NVIC_INIT_ITNS3_VAL 0x00000400`
IMPORTANT: After each code-generation check if the bit is still set or overwritten by the code-generation. 

Build and run like normal trustzone project e.g. described here https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/STM32H573I-DK/Examples/GTZC/GTZC_MPCWM_IllegalAccess_TrustZone

You should now be able to ping the board!

 

One last question: 

I need to manually change the Pinlayout of ETH to get it working, i.e. assign ETH_TXD1 to PG12.

Additionally my issue with the Interrupt where i manually need to set a bit in the files.

Are these known issues or can I report them somewhere?

Same goes for the MPCBB config, i understand that you might expect developers to do this by themselfs, but a small note when assigning ETH to NonSecure would be really nice as debugging this is kinda pain.

 

Again, thanks for your help.

Best,

funkii

15 replies

ST Employee
Nov 23, 2023 2:26 PM UTC

Hello @funkii ,

  1. what is your entry point for the non secure project ?
  2. what is done in the secure project ?
  3. are you sure that when you are pinging the board you are in non secure state and running the dedicated code for NETX ? if it's the case are you sure that you are passing the  tx_application_define() function successfully .
  4. the semaphore blocking you is  put in the  ip_address_change_notify_callback() function . try to visualise if the app is executing this function 

BR

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
funkiiAuthor
Associate II
Nov 23, 2023 5:32 PM UTC

Hi,

thank you for your reply!

My starting point is an completely empty TrustZone project. Besides the steps in the original post i do not modify anything (except for the for(;;); loops in nx_app_thread_entry()).


So for 1) I'm not really sure what you mean, so I uploaded my NonSecure main.c here. It only does the basic Init stuff and then calls ThreadX with "MX_ThreadX_Init()"

For 2) I dont really do anything in the Secure Part besides the auto-generated init stuff. I also uploaded the secure main.c here 

3) I'm not 100% sure if I'm in the nonsecure state, but I did not add any context switch to the secure state, so the board should definitely be in the nonsecure state. As this 'just works' with deactivated TrustZone i supposed that i do not need to modify anything else. What do you mean with "if it's the case are you sure that you are passing the  tx_application_define() function successfully"?, could you explain this?

4) The callback function never gets executed (tested with the debugger). For debugging reasons I added an infinite loop in the error case (Without that loop, i cannot ping the board aswell). I also tried to incrase the timeout in tx_semaphore_get() without success. I marked the spot where the execution lands in my nx_app_thread_entry 

 

So as stated earlier, I only let the IDE auto-generate the code after choosing the options in the starting point. 

If this helps, I also uploaded my .ioc file  .

I'd appreciate it if you could get into detail about what you mean in 3).

Best,

funkii

ST Employee
Nov 27, 2023 1:35 PM UTC

Hello @funkii ,

The documents that you added in your previous post can't be opened so i suggest you upload them directly into the thread in the community.

Passing now to he the third point of my previous post if are able to debug and point to the tx_application_define() and see its execution that confirms that you are in a non secure state because this code is found in the non secure project.

after giving it some thought i recommend you check the memory mapping to see if there is any secure region overlapping an non secure one and i also recommend verifying that the gpio pins of the Ethernet are assigned to the non secure project for sure as well as the other peripherals like the timer.

check if you can the address of the semaphore blocking your project  if it is in a secure or non secure memory page.

check if there is any security enabled on the flash like MPU for example .

waiting for some details on your configuration and code to help you further.

BR 

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
funkiiAuthor
Associate II
Nov 27, 2023 3:18 PM UTC

Hi,

sorry for the problem with the links, but when i click on them they take me to pastebin.

I additionally uploaded the ioc file here. I cannot upload all files in this post because of character restriction... The main.c of secure and nonsecure world are only the autogenerated files anyways, so i think the ioc file should be enough.

ioc file:

 

Spoiler
#MicroXplorer Configuration settings - do not modify
CAD.formats=
CAD.pinconfig=
CAD.provider=
CORTEX_M33_NS.userName=CORTEX_M33
CortexM33NS.IPs=CORTEX_M33_NS\:I,FILEX\:I,GPDMA1,GPDMA2,GPIO\:I,GTZC_NS\:I,LEVELX\:I,LINKEDLIST,NETXDUO\:I,NVIC2\:I,PWR,RCC,RTC,SYS\:I,TAMP,THREADX\:I,USBX\:I,SECURE_MANAGER_API\:I,ETH\:I,TIM6\:I
CortexM33NS.Pins=PH0-OSC_IN(PH0)
CortexM33S.IPs=CORTEX_M33_S\:I,GPDMA1\:I,GPDMA2\:I,GPIO,GTZC_S\:I,LINKEDLIST\:I,NVIC1\:I,OTFDEC1\:I,PWR\:I,RCC\:I,RTC\:I,SYS_S\:I,TAMP\:I,ICACHE\:I,ADC1\:I,ADC2\:I,SAI1\:I,SAI2\:I,I2C4\:I,DEBUG\:I,FMC\:I,USB\:I,USART1\:I,SDMMC1\:I,TIM1\:I,OCTOSPI1\:I,SPI5\:I,UCPD1\:I,I2C1\:I,USART3\:I,SAU\:I,MEMORYMAP\:I
ETH.IPParameters=MediaInterface,RxBuffLen
ETH.MediaInterface=HAL_ETH_RMII_MODE
ETH.RxBuffLen=1536
File.Version=6
GPIO.groupedBy=Group By Peripherals
GTZC_S.ADC_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.FMC_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.I2C1_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.I2C4_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.IPParameters=MPCBB3_SecConfig_array,ADC_Secure,FMC_Secure,I2C1_Secure,I2C4_Secure,OCTOSPI1_Secure,SAI1_Secure,SAI2_Secure,SDMMC1_Secure,SPI5_Secure,TIM1_Secure,UCPD1_Secure,USART1_Secure,USART3_Secure,USB_Secure
GTZC_S.MPCBB3_SecConfig_array=00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000\:00000000
GTZC_S.OCTOSPI1_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.SAI1_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.SAI2_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.SDMMC1_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.SPI5_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.TIM1_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.UCPD1_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.USART1_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.USART3_Secure=GTZC_TZSC_PERIPH_SEC
GTZC_S.USB_Secure=GTZC_TZSC_PERIPH_SEC
KeepUserPlacement=false
Mcu.CPN=STM32H573IIK3Q
Mcu.Context0=CortexM33S
Mcu.Context1=CortexM33NS
Mcu.ContextNb=2
Mcu.ContextProject=TrustZoneEnabled
Mcu.Family=STM32H5
Mcu.IP0=CORTEX_M33_NS
Mcu.IP1=CORTEX_M33_S
Mcu.IP10=SYS
Mcu.IP11=SYS_S
Mcu.IP12=THREADX
Mcu.IP2=ETH
Mcu.IP3=GTZC_S
Mcu.IP4=ICACHE
Mcu.IP5=NETXDUO
Mcu.IP6=NVIC2
Mcu.IP7=NVIC1
Mcu.IP8=PWR
Mcu.IP9=RCC
Mcu.IPNb=13
Mcu.Name=STM32H573IIKxQ
Mcu.Package=UFBGA176
Mcu.Pin0=PG12
Mcu.Pin1=PG13
Mcu.Pin10=VP_GTZC_S_VS_GTZC_Enable
Mcu.Pin11=VP_ICACHE_VS_SECURE_ICACHE_REG
Mcu.Pin12=VP_NETXDUO_VS_NXOoCore
Mcu.Pin13=VP_NETXDUO_VS_AddonsOoDHCP
Mcu.Pin14=VP_NETXDUO_VS_NetworkOoInterface
Mcu.Pin15=VP_NETXDUO_VS_EthernetOoPhyOoInterface
Mcu.Pin16=VP_PWR_VS_SECSignals
Mcu.Pin17=VP_SYS_VS_tim6
Mcu.Pin18=VP_SYS_S_VS_Systick
Mcu.Pin19=VP_THREADX_VS_RTOSJjThreadXJjCoreJjDefault
Mcu.Pin2=PG11
Mcu.Pin3=PH0-OSC_IN(PH0)
Mcu.Pin4=PC1
Mcu.Pin5=PA1
Mcu.Pin6=PA2
Mcu.Pin7=PC4
Mcu.Pin8=PC5
Mcu.Pin9=PA7
Mcu.PinsNb=20
Mcu.ThirdPartyNb=0
Mcu.UserConstants=
Mcu.UserName=STM32H573IIKxQ
MxCube.Version=6.9.2
MxDb.Version=DB.6.0.92
NETXDUO.ETH_ON=1
NETXDUO.IPParameters=ETH_ON,LAN_8742,NX_ENABLE_INTERFACE_CAPABILITY,NX_APP_MEM_POOL_SIZE,NetXDuo_Generate_Init_Code,NX_APP_IP_INSTANCE_THREAD_SIZE,NX_APP_PACKET_POOL_SIZE,NX_APP_THREAD_STACK_SIZE
NETXDUO.LAN_8742=1
NETXDUO.NX_APP_IP_INSTANCE_THREAD_SIZE=2*1024
NETXDUO.NX_APP_MEM_POOL_SIZE=30*1024
NETXDUO.NX_APP_PACKET_POOL_SIZE=10
NETXDUO.NX_APP_THREAD_STACK_SIZE=2*1024
NETXDUO.NX_ENABLE_INTERFACE_CAPABILITY=true
NETXDUO.NetXDuo_Generate_Init_Code=true
NVIC1.BFHFNMINS=0
NVIC1.BusFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC1.DebugMonitor_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC1.ForceEnableDMAVector=true
NVIC1.HardFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC1.MemoryManagement_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC1.NonMaskableInt_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC1.PRIS=0
NVIC1.PendSV_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC1.PriorityGroup=NVIC_PRIORITYGROUP_4
NVIC1.SVCall_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC1.SecureFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC1.SysTick_IRQn=true\:15\:0\:false\:false\:true\:false\:true\:false
NVIC1.UsageFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false
NVIC2.BFHFNMINS=0
NVIC2.ETH_IRQn=true\:7\:0\:true\:false\:true\:false\:true\:true\:true
NVIC2.ForceEnableDMAVector=true
NVIC2.MemoryManagement_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false
NVIC2.PRIS=0
NVIC2.PendSV_IRQn=true\:0\:0\:false\:false\:false\:false\:false\:false\:false
NVIC2.PriorityGroup=NVIC_PRIORITYGROUP_4
NVIC2.SVCall_IRQn=true\:0\:0\:false\:false\:false\:false\:false\:false\:false
NVIC2.SavedPendsvIrqHandlerGenerated=true
NVIC2.SavedSvcallIrqHandlerGenerated=true
NVIC2.SavedSystickIrqHandlerGenerated=true
NVIC2.SysTick_IRQn=true\:0\:0\:false\:false\:false\:false\:false\:true\:false
NVIC2.TIM6_IRQn=true\:15\:0\:false\:false\:true\:false\:false\:true\:true
NVIC2.TimeBase=TIM6_IRQn
NVIC2.TimeBaseIP=TIM6
NVIC2.UsageFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false
NetXDuo.BSP.number=1
NetXDuo0.BSP.STBoard=false
NetXDuo0.BSP.api=BSP_COMPONENT_DRIVER
NetXDuo0.BSP.component=lan8742
NetXDuo0.BSP.condition=
NetXDuo0.BSP.instance=lan8742
NetXDuo0.BSP.ip=
NetXDuo0.BSP.mode=
NetXDuo0.BSP.name=LAN_Component
NetXDuo0.BSP.semaphore=SEMA_lan8742
NetXDuo0.BSP.solution=lan8742
PA1.GPIOParameters=PinAttribute
PA1.Mode=RMII
PA1.PinAttribute=CortexM33NS
PA1.Signal=ETH_REF_CLK
PA2.GPIOParameters=PinAttribute
PA2.Mode=RMII
PA2.PinAttribute=CortexM33NS
PA2.Signal=ETH_MDIO
PA7.GPIOParameters=PinAttribute
PA7.Mode=RMII
PA7.PinAttribute=CortexM33NS
PA7.Signal=ETH_CRS_DV
PC1.GPIOParameters=PinAttribute
PC1.Mode=RMII
PC1.PinAttribute=CortexM33NS
PC1.Signal=ETH_MDC
PC4.GPIOParameters=PinAttribute
PC4.Mode=RMII
PC4.PinAttribute=CortexM33NS
PC4.Signal=ETH_RXD0
PC5.GPIOParameters=PinAttribute
PC5.Mode=RMII
PC5.PinAttribute=CortexM33NS
PC5.Signal=ETH_RXD1
PG11.GPIOParameters=PinAttribute
PG11.Mode=RMII
PG11.PinAttribute=CortexM33NS
PG11.Signal=ETH_TX_EN
PG12.GPIOParameters=PinAttribute
PG12.Locked=true
PG12.Mode=RMII
PG12.PinAttribute=CortexM33NS
PG12.Signal=ETH_TXD1
PG13.GPIOParameters=PinAttribute
PG13.Mode=RMII
PG13.PinAttribute=CortexM33NS
PG13.Signal=ETH_TXD0
PH0-OSC_IN(PH0).ContextOwner=CortexM33NS
PH0-OSC_IN(PH0).GPIOParameters=PinAttribute
PH0-OSC_IN(PH0).Mode=HSE-DIG-External-Clock-Source
PH0-OSC_IN(PH0).PinAttribute=CortexM33NS
PH0-OSC_IN(PH0).Signal=RCC_OSC_IN
PinOutPanel.CurrentBGAView=Top
PinOutPanel.RotationAngle=0
ProjectManager.AskForMigrate=true
ProjectManager.BackupPrevious=false
ProjectManager.CompilerOptimize=6
ProjectManager.ComputerToolchain=false
ProjectManager.CoupleFile=false
ProjectManager.CustomerFirmwarePackage=
ProjectManager.DefaultFWLocation=true
ProjectManager.DeletePrevious=true
ProjectManager.DeviceId=STM32H573IIKxQ
ProjectManager.FirmwarePackage=STM32Cube FW_H5 V1.1.1
ProjectManager.FreePins=false
ProjectManager.HalAssertFull=false
ProjectManager.HeapSize=M33S-0x200,M33NS-0x200
ProjectManager.KeepUserCode=true
ProjectManager.LastFirmware=true
ProjectManager.LibraryCopy=1
ProjectManager.MainLocation=Core/Src
ProjectManager.NoMain=false
ProjectManager.PreviousToolchain=
ProjectManager.ProjectBuild=false
ProjectManager.ProjectFileName=wip.ioc
ProjectManager.ProjectName=wip
ProjectManager.ProjectStructure=M33S\:Secure Project\:true;M33NS\:Non Secure Project\:true;
ProjectManager.RegisterCallBack=
ProjectManager.StackSize=M33S-0x400,M33NS-0x400
ProjectManager.TargetToolchain=STM32CubeIDE
ProjectManager.ToolChainLocation=
ProjectManager.UAScriptAfterPath=
ProjectManager.UAScriptBeforePath=
ProjectManager.UnderRoot=true
ProjectManager.functionlistsort=1-SystemClock_Config-RCC-false-HAL-false-CortexM33S,2-MX_GPIO_Init-GPIO-false-HAL-true-CortexM33S,3-MX_GTZC_S_Init-GTZC_S-false-HAL-true-CortexM33S,4-MX_ICACHE_Init-ICACHE-false-HAL-true-CortexM33S,1-SystemClock_Config-RCC-false-HAL-false-CortexM33NS,2-MX_GPIO_Init-GPIO-false-HAL-true-CortexM33NS,3-MX_ETH_Init-ETH-false-HAL-true-CortexM33NS,4-MX_NetXDuo_Init-NETXDUO-false-HAL-false-CortexM33NS,0-MX_CORTEX_M33_S_Init-CORTEX_M33_S-false-HAL-true-CortexM33S,0-MX_PWR_Init-PWR-false-HAL-true-CortexM33S,0-MX_CORTEX_M33_NS_Init-CORTEX_M33_NS-false-HAL-true-CortexM33NS,0-MX_PWR_Init-PWR-false-HAL-true-CortexM33NS
RCC.ADCFreq_Value=250000000
RCC.AHBFreq_Value=250000000
RCC.APB1Freq_Value=250000000
RCC.APB1TimFreq_Value=250000000
RCC.APB2Freq_Value=250000000
RCC.APB2TimFreq_Value=250000000
RCC.APB3Freq_Value=250000000
RCC.CECFreq_Value=32000
RCC.CKPERFreq_Value=64000000
RCC.CRSFreq_Value=48000000
RCC.CSI_VALUE=4000000
RCC.CortexFreq_Value=250000000
RCC.DACFreq_Value=32768
RCC.EPOD_VALUE=25000000
RCC.ETHFreq_Value=250000000
RCC.FCLKCortexFreq_Value=250000000
RCC.FDCANFreq_Value=25000000
RCC.FamilyName=M
RCC.HCLKFreq_Value=250000000
RCC.HSE_VALUE=25000000
RCC.HSI48_VALUE=48000000
RCC.HSIDiv=RCC_HSI_DIV1
RCC.HSI_VALUE=64000000
RCC.I2C1Freq_Value=250000000
RCC.I2C2Freq_Value=250000000
RCC.I2C3Freq_Value=250000000
RCC.I2C4Freq_Value=250000000
RCC.I3C1Freq_Value=250000000
RCC.IPParameters=ADCFreq_Value,AHBFreq_Value,APB1Freq_Value,APB1TimFreq_Value,APB2Freq_Value,APB2TimFreq_Value,APB3Freq_Value,CECFreq_Value,CKPERFreq_Value,CRSFreq_Value,CSI_VALUE,CortexFreq_Value,DACFreq_Value,EPOD_VALUE,ETHFreq_Value,FCLKCortexFreq_Value,FDCANFreq_Value,FamilyName,HCLKFreq_Value,HSE_VALUE,HSI48_VALUE,HSIDiv,HSI_VALUE,I2C1Freq_Value,I2C2Freq_Value,I2C3Freq_Value,I2C4Freq_Value,I3C1Freq_Value,LPTIM1Freq_Value,LPTIM2Freq_Value,LPTIM3Freq_Value,LPTIM4Freq_Value,LPTIM5Freq_Value,LPTIM6Freq_Value,LPUART1Freq_Value,LSCOPinFreq_Value,LSE_VALUE,LSIRC_VALUE,MCO1PinFreq_Value,MCO2PinFreq_Value,OCTOSPIMFreq_Value,PLL2FRACN,PLL2N,PLL2P,PLL2PoutputFreq_Value,PLL2QoutputFreq_Value,PLL2RoutputFreq_Value,PLL3PoutputFreq_Value,PLL3QoutputFreq_Value,PLL3RoutputFreq_Value,PLLM,PLLN,PLLPoutputFreq_Value,PLLQoutputFreq_Value,PLLSourceVirtual,PWRFreq_Value,RNGFreq_Value,RTCFreq_Value,SAI1Freq_Value,SAI2Freq_Value,SDMMC1Freq_Value,SDMMC2Freq_Value,SPI1Freq_Value,SPI2Freq_Value,SPI3Freq_Value,SPI4Freq_Value,SPI5Freq_Value,SPI6Freq_Value,SYSCLKFreq_VALUE,SYSCLKSource,UART12Freq_Value,UART4Freq_Value,UART5Freq_Value,UART7Freq_Value,UART8Freq_Value,UART9Freq_Value,UCPD1outputFreq_Value,USART10Freq_Value,USART11Freq_Value,USART1Freq_Value,USART2Freq_Value,USART3Freq_Value,USART6Freq_Value,USBFreq_Value,VCOInput2Freq_Value,VCOInput3Freq_Value,VCOInputFreq_Value,VCOOutputFreq_Value,VCOPLL2OutputFreq_Value,VCOPLL3OutputFreq_Value
RCC.LPTIM1Freq_Value=250000000
RCC.LPTIM2Freq_Value=250000000
RCC.LPTIM3Freq_Value=250000000
RCC.LPTIM4Freq_Value=250000000
RCC.LPTIM5Freq_Value=250000000
RCC.LPTIM6Freq_Value=250000000
RCC.LPUART1Freq_Value=250000000
RCC.LSCOPinFreq_Value=32000
RCC.LSE_VALUE=32768
RCC.LSIRC_VALUE=32000
RCC.MCO1PinFreq_Value=64000000
RCC.MCO2PinFreq_Value=250000000
RCC.OCTOSPIMFreq_Value=250000000
RCC.PLL2FRACN=0
RCC.PLL2N=32
RCC.PLL2P=1
RCC.PLL2PoutputFreq_Value=128000000
RCC.PLL2QoutputFreq_Value=64000000
RCC.PLL2RoutputFreq_Value=64000000
RCC.PLL3PoutputFreq_Value=258000000
RCC.PLL3QoutputFreq_Value=258000000
RCC.PLL3RoutputFreq_Value=258000000
RCC.PLLM=5
RCC.PLLN=100
RCC.PLLPoutputFreq_Value=250000000
RCC.PLLQoutputFreq_Value=250000000
RCC.PLLSourceVirtual=RCC_PLL1_SOURCE_HSE
RCC.PWRFreq_Value=250000000
RCC.RNGFreq_Value=48000000
RCC.RTCFreq_Value=32000
RCC.SAI1Freq_Value=128000000
RCC.SAI2Freq_Value=128000000
RCC.SDMMC1Freq_Value=250000000
RCC.SDMMC2Freq_Value=250000000
RCC.SPI1Freq_Value=250000000
RCC.SPI2Freq_Value=250000000
RCC.SPI3Freq_Value=250000000
RCC.SPI4Freq_Value=250000000
RCC.SPI5Freq_Value=250000000
RCC.SPI6Freq_Value=250000000
RCC.SYSCLKFreq_VALUE=250000000
RCC.SYSCLKSource=RCC_SYSCLKSOURCE_PLLCLK
RCC.UART12Freq_Value=250000000
RCC.UART4Freq_Value=250000000
RCC.UART5Freq_Value=250000000
RCC.UART7Freq_Value=250000000
RCC.UART8Freq_Value=250000000
RCC.UART9Freq_Value=250000000
RCC.UCPD1outputFreq_Value=16000000
RCC.USART10Freq_Value=250000000
RCC.USART11Freq_Value=250000000
RCC.USART1Freq_Value=250000000
RCC.USART2Freq_Value=250000000
RCC.USART3Freq_Value=250000000
RCC.USART6Freq_Value=250000000
RCC.USBFreq_Value=48000000
RCC.VCOInput2Freq_Value=4000000
RCC.VCOInput3Freq_Value=4000000
RCC.VCOInputFreq_Value=5000000
RCC.VCOOutputFreq_Value=500000000
RCC.VCOPLL2OutputFreq_Value=128000000
RCC.VCOPLL3OutputFreq_Value=516000000
VP_GTZC_S_VS_GTZC_Enable.Mode=GTZC_Enable
VP_GTZC_S_VS_GTZC_Enable.Signal=GTZC_S_VS_GTZC_Enable
VP_ICACHE_VS_SECURE_ICACHE_REG.Mode=ICACHE_REG_Not_Secured
VP_ICACHE_VS_SECURE_ICACHE_REG.Signal=ICACHE_VS_SECURE_ICACHE_REG
VP_NETXDUO_VS_AddonsOoDHCP.Mode=Addons_DHCP_Client
VP_NETXDUO_VS_AddonsOoDHCP.Signal=NETXDUO_VS_AddonsOoDHCP
VP_NETXDUO_VS_EthernetOoPhyOoInterface.Mode=LAN8742_Phy_Interface
VP_NETXDUO_VS_EthernetOoPhyOoInterface.Signal=NETXDUO_VS_EthernetOoPhyOoInterface
VP_NETXDUO_VS_NXOoCore.Mode=NX_Core
VP_NETXDUO_VS_NXOoCore.Signal=NETXDUO_VS_NXOoCore
VP_NETXDUO_VS_NetworkOoInterface.Mode=Ethernet_Interface
VP_NETXDUO_VS_NetworkOoInterface.Signal=NETXDUO_VS_NetworkOoInterface
VP_PWR_VS_SECSignals.Mode=Security/Privilege
VP_PWR_VS_SECSignals.Signal=PWR_VS_SECSignals
VP_SYS_S_VS_Systick.Mode=SysTick
VP_SYS_S_VS_Systick.Signal=SYS_S_VS_Systick
VP_SYS_VS_tim6.Mode=TIM6
VP_SYS_VS_tim6.Signal=SYS_VS_tim6
VP_THREADX_VS_RTOSJjThreadXJjCoreJjDefault.Mode=Core_Default
VP_THREADX_VS_RTOSJjThreadXJjCoreJjDefault.Signal=THREADX_VS_RTOSJjThreadXJjCoreJjDefault
board=STM32H573I-DK
boardIOC=true
isbadioc=false

 

Passing now to he the third point of my previous post if are able to debug and point to the tx_application_define() and see its execution that confirms that you are in a non secure state because this code is found in the non secure project.


If I set a breakpoint there, it the execution gets hold. So I do enter this function.

 

after giving it some thought i recommend you check the memory mapping to see if there is any secure region overlapping an non secure one and i also recommend verifying that the gpio pins of the Ethernet are assigned to the non secure project for sure as well as the other peripherals like the timer.


I double checked this a few times, everything is assigned to the NS world. (Also see the ioc file above, i hope i did not miss anything)


check if you can the address of the semaphore blocking your project  if it is in a secure or non secure memory page.

check if there is any security enabled on the flash like MPU for example .

waiting for some details on your configuration and code to help you further.


I can access it. I think the problem here is that the callback function ip_address_change_notify_callback() never gets called (observed by setting a breakpoint at function entry)

MPU is for both secure and nonsecure disabled (MPU NOT USED). What might be a problem is that i did not change anything for the GTZC config. But i suppose if the problem would be an access violation of some kind the execution would land in the hardfault handler of the secure world, so I dont think that is the case.

I appreciate your effort to help me! Thank you

Best,

funkii

 

ST Employee
Nov 27, 2023 4:49 PM UTC

hELLO @funkii ,

Could you check if the preemption priority of the Ethernet global interrupt in your msp.c in your non secure project and try and change it  maybe.

to further pinpoint the problem i recommend you start a new ioc file and implement the project from scratch and try every feature one by one because i think this is related to preemption priorities given by the threadx which can be not inline with the new  NVIC 1 and NVIC 2 attribution causing you to not ever enter the callback were the semaphore is given .

try and check if there is any interference in the priority attribution between the Ethernet and the threadx defined interrupts .

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
funkiiAuthor
Associate II
Nov 27, 2023 6:14 PM UTC

Hi @STea,

i understand that a problem with the Interrupts could be the issue.


Could you check if the preemption priority of the Ethernet global interrupt in your msp.c in your non secure project and try and change it  maybe.


I suppose you mean the file stm32h5x_hal_msp.c, i tried to change the following line there:

 HAL_NVIC_SetPriority(ETH_IRQn, 7, 0);

I used the values 0, 7, and 15 for the second and third argument, sadly with no change.


to further pinpoint the problem i recommend you start a new ioc file and implement the project from scratch and try every feature one by one because i think this is related to preemption priorities given by the threadx which can be not inline with the new  NVIC 1 and NVIC 2 attribution causing you to not ever enter the callback were the semaphore is given .

try and check if there is any interference in the priority attribution between the Ethernet and the threadx defined interrupts .


I'm not really sure if you meant that, but I tried to completely disable the interrupts in a project with disabled TrustZone (that works with enabled Interrupts). After disabling the interrupts, the same behavior can be observed. 

So i guess my problem of the initial post is somehow caused by an issues with interrupts. 

Because playing around with the interrupt priority did not change anything, do you have any suggestions what I could do? I could use another networkstack that does not rely on interrupts but only on polling, maybe that fixes that problem (Polling mode might be ugly but could work for my usecase). Do you think that might be an good idea?

Again, thanks for your help.

Best,

funkii

ST Employee
Nov 28, 2023 10:58 AM UTC

Hi @funkii ,

regarding your suggestion i do not recommend switching to a pooling mode as the interrupts are the cornerstone of any real-time system and this can affect the handling other tasks in the application .

For now i recommend you further investigate on the priority attribution for the callback and what should trigger it in the project without Trustzone enabled to identify the root cause preventing the callback from executing i will further investigate on this issue i'll keep you updated .

BR 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
funkiiAuthor
Associate II
Nov 28, 2023 8:32 PM UTC

Hi @STea ,

I observed some weird interrupt behavior. 

I currently have two projects, one without Trustzone, one with Trustzone enabled. They are configured the same way using the steps in the initial post (except assigning everything to the NS world in the TZ enabled version. Also I set the option bytes accordingly if I switch projects).

If I set a breakpoint in the "stm32h5xx_it.c" file, in the function ETH_IRQHandler(), the execution in the TZ enabled Project never holds, i.e. never reaches this point so the something is definitely wrong with the interrupts... 

In contrast, in the project without TrustZone, the breakpoint gets reached as expected.

I'll keep you updated on any news.

Best,

funkii

funkiiAuthor
Associate II
Nov 29, 2023 5:33 PM UTC

Hi,

some more observations while debugging further:

I created three Projects. In every one of them I first cleared the pinout, set the High Speed Clock under the RCC to DIGBYPASS Clock Source, enabled Ethernet to 'RMII' mode, activated the Ethernet global interrupt to preemption priority 7 and set the Pin PG12 to ETH_TXD1. Additionally I set a breakpoint in the stm32h5xx_it.c in the Ethernet Interrupt handler (In the two projects with enabled TrustZone, I set the breakpoints in the 'World' which the Ethernet is assigned to).

  1. TrustZone Disabled. Added the 'HAL_ETH_Start_IT(&heth);' to User Code 2 in main.c
  2. TrustZone Enabled. Assigned ETH to NS World. Added  HAL_ETH_Start_IT(&heth); to User Code 2 in Non Secure main.c
  3. TrustZone Enabled. Assigned ETH to S World.Added  HAL_ETH_Start_IT(&heth); to User Code 2 in Secure main.c

In 1) and 3), as expected, the breakpoint gets triggered.

In 2) the breakpoint does not get triggered for some reason. 

Does anyone have a clue why this is the case? Between switching from TZ enabled/disabled I only set the following option bytes as follows:
- TZEN=0xB4

- SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F meaning all 128 pages of Bank1 set as secure

- SECWM2_PSTRT=0x1 SECWM2_PEND=0x0 meaning no page of Bank2 set as secure, hence Bank2 non-secure

 

Best, 

funkii

 

edit:

I wrote above that the breakpoint in 1) and 3) gets triggered, which is the case. 

For some reason the Interrupt gets only called once. The Interrupt is because of an DMA Error, the DMAErrorCode gets set to ETH_DMACSR_RBU and ETH_DMACSR_AIS... Im not really sure what this means, but i guess its some kind of configuration bug because i just call HAL_ETH_Start_IT() and doesnt really matter for the initial problem.

 

 

funkiiAuthor
Associate II
Dec 5, 2023 11:53 AM UTC

Hi everyone,

some more additional information that might be relevant:

If I activate e.g. the "RCC non-secure global interrupt" in the ioc file, the file "Secure/Core/Inc/partition_stm32h573xx.h" gets changed correctly. -> I attached the git diff

@@ -386,7 +386,7 @@
 // <o.6> FLASH_IRQn <0=> Secure state
 // <o.7> FLASH_S_IRQn <0=> Secure state
 // <o.8> GTZC_IRQn <0=> Secure state
-// <o.9> RCC_IRQn <0=> Secure state
+// <o.9> RCC_IRQn <1=> Non-Secure state^M
 // <o.10> RCC_S_IRQn <0=> Secure state
 // <o.11> EXTI0_IRQn <0=> Secure state
 // <o.12> EXTI1_IRQn <0=> Secure state
@@ -410,7 +410,7 @@
 // <o.30> GPDMA1_Channel1_IRQn <0=> Secure state
 // <o.31> GPDMA1_Channel2_IRQn <0=> Secure state
 */
-#define NVIC_INIT_ITNS0_VAL 0x00000000
+#define NVIC_INIT_ITNS0_VAL 0x00000200^M

But if I activate the "Ethernet global interrupt", nothing changes in that file. I do not see any Interrupts for the ETH there at all that could be configured by hand.

Overall between activated and deactivated Interrupt, nothing at all changes in the secure subproject.

 

I think that might be the problem that I do not receive Interrupts with activated TrustZone. 

Since I'm not 100% sure that this is the problem, can anyone with more experience confirm that this is the case?

 

 

funkiiAuthor
Associate II
Dec 5, 2023 9:54 PM UTC

Hi,

there seems to be a bug in the code generation:

I looked up the Ethernet Interrupt Number in the reference manual, which is 106.

If I modify the Secure/Core/Inc/partition_stm32h573xx.h by hand and set the bits by hand my breakpoint finally gets triggered. In NVIC_INIT_ITNS3_VAL the 12th bit needs to be set.

#define NVIC_INIT_ITNS3_VAL 0x00000400

Unfortunately this does not fix my problem...

The Interrupt gets triggered once, and with a DMA Error. More accurate the Receive Buffer Unavailable (RBU) Bit gets set, together with the Abnormal Interrupt Summary (AIS). The AIS gets always set when RBU gets set.

I found this description of RBU:

This bit indicates that the application owns the next descriptor in the Receive list, and the
DMA cannot acquire it. The Rx process is suspended. To resume processing Rx descriptors,
the application should change the ownership of the descriptor and issue a Receive Poll
Demand command. If this command is not issued, the Rx process resumes when the next
recognized incoming packet is received. In ring mode, the application should advance the
Receive Descriptor Tail Pointer register of a channel. This bit is set only when the DMA owns
the previous Rx descriptor.

 

Anyone got an idea why this is happening? Do i need to change any addresses because I use TrustZone? 

Best,

funkii

ST Employee
Dec 6, 2023 9:12 AM UTC

Hello @funkii ,

When TZ enabled the ETHERNET DMA cannot acquire the descriptors (Tx Descriptor Unavailable / Rx Descriptor Unavailable) placed in SRAM. And thus whether the ETH is placed in secure or not-secure project. so you need to reconfigure the memory layout to get the descriptors out of the protected area .

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
funkiiAuthorBest answer
Associate II
Dec 7, 2023 10:06 AM UTC

Hi,

i finally managed to get it working! Thanks @STea for your help, I really appreciate it.

Steps to get it working:

Start Board Project with Trustzone enabled
Firmware Version v1.1.1

Clear pinout

ETH
 Mode RMII
 RxBuffLen 1536
 Set Pin PG12 to ETH_TXD1 (By doing this, PG14 should be cleared)

THREADX
 Core

NETXDUO
 NX Core
 Addons > DHCP > Client
 Network Interfaces > Ethernet interface, Ethernet Phy Interface > LAN8742
 Platform Settings > both lan8742

 Enable Interface Capability true
 memory pool size 30 * 1024
 Genreate Init Code true
 IP Instance Thread Size 2 * 1024
 Pool Size in number of Packets 10
 Application Thread Stack Size 2 * 1024

NVIC_NS
 Ethernet global Interupt > Enable, Preemption Priority 7

SYS
 Timebase Source TIM6 (Assign TIM6 to NS before)

RCC
 High speed Clock DIGBYPASS Clock source

GTZC_S
 Block-Based Memory Controller > MPCBB3 (SRAM3) > Memory Privilege Attributes Settings > Configure Memory > from full Not privileged
 (Setting the whole SRAM3 to not priviliged might not be the best idea from an security standpoint if you do other stuff on the board)

Manual change in Secure/Core/Inc/partition_stm32h573xx.h:
Set the 10th bit in NVIC_INIT_ITNS3_VAL (in my case line 554), so the line should look like this:
`#define NVIC_INIT_ITNS3_VAL 0x00000400`
IMPORTANT: After each code-generation check if the bit is still set or overwritten by the code-generation. 

Build and run like normal trustzone project e.g. described here https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/STM32H573I-DK/Examples/GTZC/GTZC_MPCWM_IllegalAccess_TrustZone

You should now be able to ping the board!

 

One last question: 

I need to manually change the Pinlayout of ETH to get it working, i.e. assign ETH_TXD1 to PG12.

Additionally my issue with the Interrupt where i manually need to set a bit in the files.

Are these known issues or can I report them somewhere?

Same goes for the MPCBB config, i understand that you might expect developers to do this by themselfs, but a small note when assigning ETH to NonSecure would be really nice as debugging this is kinda pain.

 

Again, thanks for your help.

Best,

funkii