Skip to main content
Yadav
Associate III
July 8, 2018
Question

Need suggestion for choosing microcontroller

  • July 8, 2018
  • 3 replies
  • 788 views
Posted on July 08, 2018 at 15:06

Hi Everyone,

     I am thinking of designing wireless home automation product using IoT. Can anyone suggest which STM32 series is suitable for this application. I have knowledge in stm3f4 series. So i can easily learn whatever series which is suitable my application.

#stm32-nucleo-64 #stm32-c2c
    This topic has been closed for replies.

    3 replies

    Bogdan Golab
    Lead
    July 8, 2018
    Posted on July 08, 2018 at 15:14

    You may want to see this board to see if it meets your needs:

    https://www.st.com/en/evaluation-tools/b-l475e-iot01a.html

     

    Actually two versions of this board exit (different radio types).

    If you think about F4 line, consider the L4 (newer, low power, etc). The board above uses L4 MCU.

    Tesla DeLorean
    Guru
    July 8, 2018
    Posted on July 08, 2018 at 15:21

    It is a multi-faceted decision, and going to be dependent on your exact requirements.

    For new designs consider the L4(+) or F7 depending on the amount of horse-power your application needs.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    T J
    Senior III
    July 9, 2018
    Posted on July 09, 2018 at 02:37

    if you would like a complete solution in one Dev board, you could look at the B-L072Z-LRWAN board.

    F series, Vs L series, Vs  F4 , when I use the cube it is all seamless....

    any chip/board will do... depending on your power budget.