Skip to main content
SKuma.4
Visitor II
November 2, 2018
Question

Need simple code on i2c for stm32f051

  • November 2, 2018
  • 2 replies
  • 636 views

..

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    November 2, 2018

    Some pretty simple stuff here that should work on an F051 based board

    STM32Cube_FW_F0_V1.9.0\Drivers\BSP\STM32F072B-Discovery\stm32f072b_discovery.c

    STM32Cube_FW_F0_V1.9.0\Drivers\BSP\STM32F072B-Discovery\stm32f072b_discovery_eeprom.c

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    T J
    Senior III
    November 3, 2018

    super simple, do you use the cube ?

    I had to write code for a 4port DAC.

    Everyone knows IIC can be problematic, however, this worked first time without any initialisation other than enabled in the cube.

    //#define MCP4728_DacAddress 0x60 << 1
    void write4Dacs(void) {
     
     struct DacIIC MCP4728IIC; 
     HAL_StatusTypeDef IIC_Response;
     
     //Channel 0
     MCP4728IIC.DacTxBuffer[0] = (Dac0_Value & 0x0f00) >> 8; // Dac0Value adjusted in another process..
     MCP4728IIC.DacTxBuffer[1] = Dac0_Value & 0x00ff;
     
     //Channel 1
     Dac1_Value = Dac0_Value + (4096 * 1) / 5; // 1V // test DAC2
     MCP4728IIC.DacTxBuffer[2] = (Dac1_Value & 0x0f00) >> 8;
     MCP4728IIC.DacTxBuffer[3] = Dac1_Value & 0x00ff;
     
     //Channel 2
     Dac2_Value = Dac1_Value + (4096 * 1) / 5; // 2V
     MCP4728IIC.DacTxBuffer[4] = (Dac2_Value & 0x0f00) >> 8;
     MCP4728IIC.DacTxBuffer[5] = Dac2_Value & 0x00ff;
     
     //Channel 3
     Dac3_Value = Dac2_Value + (4096 * 1) / 5; // 3V
     MCP4728IIC.DacTxBuffer[6] = (Dac3_Value & 0x0f00) >> 8;
     MCP4728IIC.DacTxBuffer[7] = Dac3_Value & 0x00ff;
     
     
     //DAC_IIC.write(DAC_ADDR + (Dac_Address << 1), buf, 8); //MBED write
     IIC_Response = HAL_I2C_Master_Transmit(&hi2c1, MCP4728_DacAddress, &MCP4728IIC.DacTxBuffer[0], 8, 10); 
    }